Other Parts Discussed in Thread: CC2640 1: How do I enable the TI-RTOS Object Viewer (ROV) in IAR?
A: The ROV can be enabled under the application's Project Options -> Debugger -> Plugins tab. Select " TI-RTOS " in the scroll list.
2: Why does my…
Other Parts Discussed in Thread: BLE-STACK , CC2650RC , CC2650 ble_sdk_2_02_01
1. CCS cannot find target config file for simple_peripheral_cc2650em_app project.
A: To fix this, open your project properties and select "General". Check the box marked…
General known issues and fixes, this applies to cc13xx and cc26xx
1. Device does not restart after successful OAD
A: Unplug/replug or hard reset will fix this and the device will boot okay.
There is a bug with the emulation tools packages that predate…
Part Number: CC2640R2F
IAR + Autosized heap workaround
This workaround applies to all using BLE(5)-Stack + TI-RTOS Runtime Object Viewer (ROV) for IAR with OSAL heapmgr and autosize.
Note ROV2 for CCS is not affected. This issue doesn't affect cc13x2_26x2…
Part Number: CC2640R2F
simplelink_cc2640r2_sdk_3_30_00_20
1. [BTool] Discovered devices list is never cleared
2. The following configurations are not available for host test:
peripheral + observer
central + broadcaster
peripheral + central…
Here is the overview to all the known issues and fixes.
This known issues and fixes are categorized as devices specific and components(OAD, RTLS, IDE).
Before you post any questions, please take a look at the corresponding posts. You might already…
Part Number: SIMPLELINK-CC2640R2-SDK
simplelink_cc2640r2_sdk_3_40_00_10
0. [RTLS_Monitor] We do not release anymore RTLS_Monitor. Instead, we provide a new user interface (UI) stored in your SDK in tools\ble5stack\rtls_agent\rtls_ui. Execute rtls_ui…
Part Number: TPS2373 Other Parts Discussed in Thread: TPS23880
Hi,
I'm designing a .bt PoE 5-port switch with an ideal rectifier bridge.
I want to use the PG pin, with a 10k ohm pull-up to 3.3V (one of the power supply outputs). It will trigger…
Part Number: DS125DF111 DS125DF111 is locked and you want to know what is the data rate that device is locked at. What are the settings to determine DS125DF111 locked rate?
Part Number: LP2985 Other Parts Discussed in Thread: TLV757P , TPS764 , , TLV755P , TLV767 , TPS7A26 , LP5907 , TPS709
Hi,
The datasheet states that the ON/OFF pin must be driven with a slew rate greater than 40mV/us. What is the potential concern…