Part Number: LM5109
There have been questions regarding the differences between the LM5109A and LM5109B 100V high-side low-side drivers.
The pinout, available packages and parameter specifications are the same for the LM5109A and LM5109B. So the LM5109B…
Part Number: AWR1642BOOST Other Parts Discussed in Thread: AWR1642
Tool/software: Linux
Hello,
I have completed the ROS demo using the 2.0.0.4 SDK on the AWR1642BOOST. The unit is flashed with the Demo binary file from the SDK.
I was working…
Other Parts Discussed in Thread: TLV9064 , TLV9004 , TLV9001 , TLV9062 , TLV9061 , TLV9002 Hello,
I need to identify replacement op amps for the MCP6001, MCP6002, and MCP6004 devices. What are the best replacement amplifiers from TI?
Thanks!
Hi all,
Thanks for the reply, it worked last time but now i cant figure out why the attached circuit cant be simulated and it shows some error which i cant figure out. it shows a node error between c1 and c2. please do let me know if there are any …