Part Number: TDA4VM
Tool/software:
I'm using the TDA4VM Linux or Linux+RTOS 8.6 SDK. What parameters or patches are available to be enable I-frame period and IDR frame period?
Part Number: AM62A7 Tool/software: Currently on the AM62A TI EVM, we have a OSPI Serial NAND Flash from Winbond.
The flash is: W35N01JWTBAG
Let us understand how the BBM is done with respect to some specific registers.
Part Number: PROCESSOR-SDK-AM62X
Tool/software:
In MCU+ SDK, during Flash Initialization, we read the device id and manufacture id.
Most common failure is " Unable to read Flash ID... "
Let us understand what parameters does the API Flash_norOspiReadID…
Part Number: TDA4VH-Q1 Tool/software: I want to be able to build and test the GPU test-application lightweight-offscreen demo shown here: https://github.com/StaticRocket/lightweight-offscreen
I am currently on SDK 9.2 how can I do this?
[Click here to return to Transceiver Homepage]
Welcome to the IO-Link Transceivers E2E page!
Listed below are a variety of resources to assist with the implementation of IO-Link!
IO-Link Basics:
IO-Link Overview
IO-Link Sensor Transmitter…
Part Number: AM625
Tool/software:
The Keywriter is an application designed primarily for programming the keys and converting the device from HSFS to HSSE.
During the keywriting procedure, one may encounter errors reflected by the non-zero value…
Part Number: SK-AM62A-LP
Tool/software:
Hi experts,
On SK-AM62A-LP EVM, GPIO0_12 is used for OSPI reset signal.
Why does TI not use dedicated OSPI reset pin for the purpose?
What is the TI recommendation for customer?
Best regards…