FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
TXG devices (both push-pull and open-drain) cannot support any level of IEC-ESD. However, IEC-ESD can still be achieved by using a protection device like the ESDS30x product…
Other Parts Discussed in Thread: TXG8122-Q1
Open-Drain Architecture
For I2C applications, the allowable distance between systems is primarily limited by total bus capacitance. The I2C specification limits bus capacitance to 400pF for Standard and…
FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
At the moment TXG QFN packages do not support wettable flanks. However, we are working towards supporting wettable flank packages once products are fully released.
The QFN…
Other Parts Discussed in Thread: TXG1041 FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
The leakage between two grounds is specified in the Electrical Characteristics section in the device datasheet.
The table below shows…
FAQ: Logic and Voltage Translation > Ground-Level Translators >> Current FAQ
The TXG product family can be used as a standard level translator (VCCA > VCCB or VCCA < VCCB) or in a buffer configuration when VCCA equals VCCB.
If ground shifting is not…
Part Number: MCU-PLUS-SDK-AM263X Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi TI experts,
I'm trying to run the sbl_qspi_enet application on AM263x. I see that the documentation ( software-dl.ti.com/.../EXAMPLES_DRIVERS_SBL_QSPI_ENET_AM263X…
Part Number: BQ25798 Tool/software: Backup mode is expected to work as follows:
Host software sets (arms) EN_BACKUP=1 while input source is attached at VBUS
Input voltage fails below backup mode trigger point = %*VINDPM
Backup mode engages setting…
Part Number: TXE8116-Q1 Other Parts Discussed in Thread: TCAL6416 , TXE8124 , TXE8148 , TXE8116
Tool/software:
FAQ: Logic and Voltage Translation > SPI I/O Expander >> Current FAQ
Both I2C and SPI I/O expansion solve the fundamental problem of I…
Part Number: MSPM33C321A Tool/software: 1. Background
If there is a display, then you can use it to play 'bad apple'
Now MSPM33 Launchpad has a 128*32 OLED on the board...
2. Demo video:
3. Required hardware/software
Hardware
LP-MSPM33C321A…
Part Number: CC2745R10-Q1 Tool/software: Issue:
When trying to flash or debug a CC27XX using CCS 20.3.0, the following error is reported:
Cortex_M33_0: Flash loader: CC23xx_CC27xx_FLASH_LIBRARY_VERSION 4.1.0.141
GEL: Error while executing OnPreTargetConnect…