Part Number: AM263P4-Q1 Other Parts Discussed in Thread: UNIFLASH
This FAQ explains how to setup the flash utility to flash into external flashes which are not supported out of the box. The method mentioned in this FAQ would be the same for AM261 and…
Part Number: TDA4VH-Q1
How to enable the constant monitoing of the linux and remotecores of main domain from mcu domain core (mcu1_0)?
If core is crashed and detetion is done by monitoring, how to enable autonomous recovery?
Part Number: TDP2004
This Master FAQ lists serves as a point of reference to find all FAQs made by TI's signal conditioning Team.
DPHY: 1. [FAQ] SN75DPHY440SS: Is it okay to swap the polarity and lane order? - Interface forum - Interface - TI E2E…
Part Number: AM625
What this FAQ covers? This FAQ demonstrates how to boot Linux on the AM62x SK EVM with 256 MB of DDR instead of the default 2 GB. It provides the complete set of firmware, bootloader, device tree, and kernel changes required.
Part Number: MSPM0-SDK
This thread is used to update the software or hardware update for application note of Single Phase AC Power Monitor with MSPM0
Hardware_Software.zip
Other Parts Discussed in Thread: C2000WARE , SYSCONFIG
This post is meant to specify erratas /document any refinements or clarifications discovered after the C2000Ware release.
Sysconfig migration/Switch feature in Sysconfig 1.26 does not work with…
Part Number: AM6548 Other Parts Discussed in Thread: TMDX654IDKEVM , UNIFLASH , DRA80XMEVM
Hello,
we experience problems booting an AM6548 from an eMMC in our custom board. Exactly the same binary, that is booting on the evaluation board (TMDX654IDKEVM…
Part Number: TDA4VL-Q1 Other Parts Discussed in Thread: TDA4VL , TDA4VH
When using the MCU_ADC0 or MCU_ADC1 on TDA4VL or TDA4VH, the voltage measured on ADC0_AIN7 or ADC1_AIN7 has a higher voltage than expected (i.e., for an expected voltage of 0.8V…
This serves as a selection guide for our automotive-grade devices and outlines the typical protocols associated with these devices.
1:1
2:1
3:1
4:1
8:1
SN74LVC1G66-Q1
SN74LVC2G66-Q1
TMUX7212…