Part Number: CC2538 Other Parts Discussed in Thread: Z-STACK , SEGGER , , CC2530 Hello Guys,
I successfully flashed the dongle program using the option (Download and Debug) , Then I opened OTA server PC Tool. In that, I gave all the parameters and select…
Part Number: CC1352P Other Parts Discussed in Thread: Z-STACK Hello everybody
I Have three questions with z-stack for CC1352P
1.Is it possible to perform zigbee communication on 915 MHz frequencies, or it only allows to perform zigbee communication on…
I want to use Z-Tool through UART_USB. I tried ZNP with HAL_UART_USB and USB_SETUP_MAX_NUMBER_OF_INTERFACES=5 enabled and it works, but when I do the same in GenericApp not only it doesn't work but also it doesn't recognize the device in device manager…
Part Number: CC2651P3 Hi, I'm doing a project involving Zigbee comunications, with TI boards. I been working with Ztool and ZNP proyect.
I would like to know if its possible to send the same comands as in Z-tool but from my pc shell via serial comunications…
Part Number: CC1352P Other Parts Discussed in Thread: SYSCONFIG Dear Sir or Madam,
An ZNP example (SDK 6.40) was built by IAR8.40.
SYSCONFIG_ROOT = c:/ti/sysconfig_1.15.0 in Configure Custom Argument Variable.
"Cannot specify --board without--product"…
Part Number: CC2538-CC2592EMK Other Parts Discussed in Thread: CC2538 , Z-STACK , CC2592 , CC2590 I want to amplify the original CC2538 output power, so I bought CC2538-CC2592.
I download my original code, and test the output power, it is only -94--95dBm…
Part Number: CC2538 Hi team,
The customer wants to know the meaning of the following code in hal_ota.c:
typedef long (* volatile HAPI_CRC32_T)(unsigned char *, unsigned long);
#define HAPI_CRC32_FUNC_PTR 0x00000048
#define P_HAPI_CRC32 ((HAPI_CRC32_T…
Part Number: CC2652P Chip :CC2652P1F
SDK: CC13x2 / 26x2 SDK
Demo:ZNP
Requirement:
I use CC2652 as a ZC. When I reset the ZC, it return back to DEV_HOLD
Step:
I use CC2652 as a ZC,for connecting a Zigbee light.
ZTOOL reported this warning information.…
Part Number: CC2538 Other Parts Discussed in Thread: Z-STACK Hello All
I'm trying to mode an old device based on CC2538 running Z-Stack 3.0.2 to be able to join to old HA network .
I saw that it is possible using old style commissioning. Is there any…