Hi Jacob,
TI has released TI 15.4 Stacks, available within TIMAC (deprecated) and the SIMPLELINK-LOWPOWER-F2-SDK (recommended), however TI has not invested in development of a specific Wireless HART solution and thus further user development would be…
Hi Viktorija,
We do not really have such a comparison. WHART is of course designed specifically for the application you ask for, but there is currently no support for it on our devices.
Cheers,
Fredrik
Hi,
while the CC2538 is a device capable of supporting WHART stack, TI-MAC API don't support channel hopping or TDMA WHART framing.
Thanks,
TheDarkSide
I am not able to get the SW UART to work on the Beaglebone black and I am not sure what I am issing.
Board: Beaglebone black
Base Image : am335x-debian-11.7-iot-armhf-2023-09-02-4gb
I have successfully compiled and installed a new kernel, with the…
navaneetha kothapalli said:
I would like to know whether you have wireless hart protocol stack for any of your ti controller.
I want to implement Wireless HART protocol in ti controller.
Is this a separate question or related to using the LTP5902…
Hi Hernan,
Yes, the CC2530DK can transmit Wireless HART frames using the TIMAC, but I don't know of anybody who offers a WHART stack to run on the CC2530. So you can inject pre-formatted packets, but not build an actual WHART device.
Peder
Other Parts Discussed in Thread: OPA188 , OPA237 , OPA140 , LM7705 , OPA2188 , OPA2140 Hello Everybody.
Im currently evaluating 3 op amps in Single Power supply mode, while connecting the in+ to GND and in follower mode I got aprox 8mV in the output…