Part Number: TDA4VM Other Parts Discussed in Thread: CSD Tool/software: 1、We took a high and low temperature pressure test for 16 hours and found that our sleep file was damaged after the pressure test root@j721e-evm:~# ls -l /bin/
[ 7052.671361] EXT4…
Hi Jim,
I am concerned that DP83867 may be linking up in 100Mbps instead of 1000Mbps, which is the requirement for media conversion using the DP83TG720EVM.
Can you please read PHY_ID = 00, Register Address = 0011 on both EVMs and ensure let me know the…
Part Number: AM623
Tool/software:
Hi Krunal & TI team,
Good Day!
As informed to Krunal & TI team in email communications, we would like to use the Quad SPI Serial Nand Flash interface with a density of 2G-bit (i.e. 256MB) in-order to work with…
For anyone else who comes looking at this thread, I have not been able to make this work.
Things I've tried:
ADC (slave to XMOS MCU as stand in for GAP9) in TDM
16, 24, and 32 bits @ 48/44.1kHz
ADC (still slave to the XMOS) in I2S
16, 24, 32…
Part Number: TPLD1201 Tool/software: Hi team,
Once the OTP memory of the TPLD1201 is programmed using InterConnectStudio, it becomes a permanent program and cannot be rewritten. Is this understanding correct?
During the design phase, you are configuring…
Part Number: SK-AM62B-P1 Tool/software: I have built the image for am62xx using yocto "software-dl.ti.com/.../Overview_Building_the_SDK.html" .
1.Now I when i use gpiodetect , I get gpiochip0, gpiochip1,gpiochip2
gpiodetect gpiochip0 [600000…
Hi Brian,
For the 12V/8.3A design, take a look at the LM5146 EVM, https://www.ti.com/tool/LM5146-Q1-EVM12V . This EVM is 12V/8A at Fsw = 400kHz using 100V MOSFETs. Note that an 80V controller may be somewhat tight for a 75V max Vin, hence the recommendation…
Hi Bjorn,
The I2C flow (reset chip, writing to the configuration register 1 to enable temperature sensor mode, start conversions, read conversion data) mentioned seems correct, make sure you are following the read conversion data sequence (shown below…
Part Number: J722SXH01EVM Other Parts Discussed in Thread: AM67A Tool/software: Hi,
we are having trouble toggling the GPIOs on the AM67A EVM. We've tried three GPIOs so far:
Pin17 on J33 (22Pin CSI camera port): GPIO0_15
Pin18 on J33 ( 22Pin CSI…