Part Number: 2MTR-DYNO Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM , Hi Team,
A customer has 2MTR-DYNO evaluation kit. The M-2310P-LN-04K motor included in the kit is rated at 60V, 7.1A. However, the BOOSTXL-DRV8305EVM driving the motor is rated at…
Part Number: 2MTR-DYNO
Tool/software: Code Composer Studio
Dear team,
The customer just bought it recently and received it.
One of the motors cannot rotate freely, and one of the rotors cannot be turned manually without power.
It is suspected that it…
Part Number: 2MTR-DYNO Dear all,
Now I am using 2MTR-DYNO, but I cannot find the parameters of the motor position sensor on the TI website, etc.
I urgently need to know the accurate relative relationship between the position sensor and the rotor. It mainly…
Part Number: 2MTR-DYNO Other Parts Discussed in Thread: SFRA , INA240 Hello,
I am working with the 2MTR Dyno kit and trying to control a single motor with the Launchpad and the 3ph GaN Inv. I am following the application report titled "Dual-Axis Motor Control…
Part Number: 2MTR-DYNO Hi Team,
I order the 2MTR -DYNO From TI. When I check the accessories which included with it , I have seen tow different shaft coupler. I am not able to couple both motors. I think one shaft copler size is 9.5mm and other maybe…
Other Parts Discussed in Thread: 2MTR-DYNO , LAUNCHXL-F28379D , BOOSTXL-3PHGANINV Hello,
I'd like to add TI's LVACIMTR induction motor to my collection of: (1) 2MTR-DYNO, (1) LAUNCHXL-F28379D, and (2) BOOSTXL-3PHGANINV. I know that in the past TI had kitted…
Part Number: 2MTR-DYNO Other Parts Discussed in Thread: LAUNCHXL-F28379D Good evening,
I am using the 2MTR-DYNO kit with the TI F28379D LaunchPad with 2 BOOSTXL-DRV8305 booster packs.
The code that i load on the board is obtained by playing the Simulink…
Part Number: 2MTR-DYNO
Hi Everyone,
I am working on the modeling of Dyno motor. So, I will be very pleased if anyone could provide me with any of the machine parameters such as: air-gap length, permanent magnet thickness, number of winding turns and…
Part Number: 2MTR-DYNO Other Parts Discussed in Thread: SFRA Hello,
I have a 2MTR_DYNO evaluation kit, and I am experimentig with the code.
I noticed that in the initialization of the encode peripheral, in "FCL_SFRA_XL_DualServo.c" at line 332 there is…
Part Number: 2MTR-DYNO Hi Everyone,
I am working on developing the mathematical model of the Dyno motor. So, I will be very pleased if anyone could tell me how to calculate the magnetic flux constant from the back EMF constant, which is equal to 4.64 Vpeak…