Part Number: MMWCAS-DSP-EVM I get this error after loading the meta image from the DFP and clicking 'RF Power-up' in mmWave Studio 2G. Anyone seen this before?
Part Number: DS90UB941AS-Q1 Hi experts,
Can I ues 941 register-only GPIO (GPIO_REG[8:5]) to control 948 GPIO_REG[8:5]? For example, if I want to send data from 941 GPIO8_REG to 948 GPIO8_REG, is below code correct? Any other configuration is required…
Part Number: TUSB2077A Greetings,
I have a question regarding the TUSB2077A.
In my customers application, pin 47 () is always tied to logic high (3.3v) and they'd like for the overcurrent detection to be in ‘ganged’ mode.
What logic level For…
Part Number: ADS1299-4 Hi,
We are currently using the ADS1299-8 channel and have populated all 8 channel inputs using an RC circuit, as per the datasheet.
We would like to swap out the 8 channel with a 4 channel chip (ADS1299-4) and would like to…
Part Number: TMS320F280049
Dear guys,
I wonder what the title of the first column means in the table attached below. "0,4,8,12" means what? I know that the first column lists the sequential GPIOs, but "0,4,8,12" ??
Hope someone can answer me.…
Part Number: TPS25947
hello team:
in the datasheet of tps25947,Table 8-5 mentions some PG output states. in some cases, only the PG state is mentioned when the PGTH pin voltage is less than Vpgthf, and the state when the PGTH voltage is greater than…
Part Number: PROCESSOR-SDK-AM437X How to implement Linux lcd driver by referring to idk, since the pin lcd interface needs to use 8-bit RFBI asynchronous mode?
Other Parts Discussed in Thread: LMG1020 , CSD17571Q2 , CSD15571Q2 , CSD16301Q2 Dear sir ,
i want to create a signal from Arduino Due at 5MHZ (a square wave ) 50% duty cycle to be connected to fast gate controlled mosfet(NPN) to switch a load 12 volt…
Part Number: SN74LVC1G125 Other Parts Discussed in Thread: SN74LVC1G240 , , SN74LVC2G241 , SN74LXC1T45 Dear TI support team,
I am struggling with a very strange problem. I would like to have a 3.3 V MCU communicate on a 5V SDI-12 bus (cf. https://sdi…
Part Number: SN74LVC1G32 Other Parts Discussed in Thread: 5-8-LOGIC-EVM Tool/software: My customer is looking for some insight into the following regarding the data sheet.
In page # 6, do I need to add these lumped components?, if so could you provide…