Part Number: TMS320F28388D Other Parts Discussed in Thread: OPA320 , OPA4322-Q1 Hello,
This question is regarding the oscilloscope measurement below. The measurement is the voltage seen at the SAR ADC input pin of the processor (pin 39, ADCINA4) during…
Part Number: TMS320F28377D-EP Hello there,
I am planning to use the 176-Pin F28377D and would like the higher 16-bit resolution with a single-ended input. I was hoping for some clarity regarding this third note. Could someone provide an explanation…
Part Number: ADS8688 Hi,
We are planning to implement Multilevel thersholding using ADC, whereas my input will be in DC voltage from the rf detector, so will my ADC accept DC voltage and provide the sampling data?
RF detector (Vout of Rf detector…
Part Number: AM263P4-Q1 Hello,
datasheet SPRSP81D lists for ADC_R:
Input Conversion Range (Vin+, Vin-) Must be < VDDA33 min: 0 max: 33 /18 × VREFHI
But in realitiy >=3.2V (single ended) result in 4095, so is the datasheet wrong or am I just missunderstanding…
Part Number: THS4551 Other Parts Discussed in Thread: ADS1278 , THS4552 Hey , am designing a board with ads1278 24bit 8 channel adc , and i have very limited space and budget , I was wondering if I can drive four of the ads1278 inputs with one single…
Part Number: MSPM0-SDK Other Parts Discussed in Thread: MSPM0C1104 , SYSCONFIG For a project I need to use the ADC of the MSPM0C1104 to read different analog inputs in sequence mode. In the datasheet it said upto 10 channels. However when I create a new…
Part Number: AMC3330 Other Parts Discussed in Thread: AMC0230D , AMC1311 , , AMC1350 , ISO224 , AMC0211D I am designing an isolated ADC circuit and would like to verify my front-end configuration.
My application requires measuring a range of -50V to…
Part Number: AM2612-Q1 Other Parts Discussed in Thread: AM2612
have the AM261 launchpad eval board.
planning on using the AM2612 for future automotive projects,
WE have been using (and still do use) the TMS570 Hercules.
Per data sheet AM2612:…
Part Number: AM6442 Tool/software: Hello, We have dseigned a custom board based on AM6442 where we are using 8 channel ADC's. Here we have observed few things as below
When there is no input voltage supplied and the pin is left floating we see a reading…
Part Number: ADS8688A Table 1 of the datasheet states that if the Input voltage is between the Vrange and Vovp, the ADC output will be saturated. It states that the device is internally progected but this state is not recommended for extended time. Can…