Part Number: MSPM0G1506 Hello. My name is Mori. I'm looking for a way to measure internal VREF using an ADC. The calculation formula is as follows. Measure the internal VREF using VDDA as the reference voltage.
(Vref/VDDA)×4095 = measured value…
Part Number: LP-MSPM0L1306 Other Parts Discussed in Thread: SYSCONFIG Hi Team!
I'm trying to use an external reference of 2 V with the VREF module and ADC. I'm using example code adc12_single_conversion_vref_external as the starting point.
Software…
Part Number: BQ76940 Hi,
I want to do a thyrocervical calculation for ADC accuracy for comparison with the practical measurement of AFE Cell voltage, so I am not getting any Vref- "14 Bit ADC reference voltage for calculation" Please give me information…
Part Number: MSPM0G3507 Other Parts Discussed in Thread: SYSCONFIG
Vref- not used, this pin is used as an ADC pin, and the reference source of ADC is set to Vref. When the voltage of the ADC pin where Vref- is located changes, the sampling values of other…
Sagar Dudhal said: So my resolution will be Vref/4096= 2.048/4096= 500uV
or
3V/4096= 732uV
The resolution is always 732mV regardless of what reference mode you use.
Sagar Dudhal said: Does this TMS320F2883 is designed in such a way that it it will give…
HI Kagen,
Unfortunately, I can only make proper suggestions for audio devices since these are the IC's I specialize in. Please create another thread with MCU and processors team so their experts can properly assist you.
Kind regards,
Part Number: ADS1246 Other Parts Discussed in Thread: ADS124S08 , , ADS124S06 Hello,
I'm looking for an ADC to fit the following specifications.
It has to measure a PT1000 RTD from a range of -50degC to 300 degC with a precision of 0.001 degC across…
Part Number: TMS320F280039C Hi Team,
We want to know is which one has better performance when 280039C uses the internal 2.5V reference or the 3.3V reference?
How much difference will there be in performance?
Best Regards,
Zane