Part Number: TPS650864 Other Parts Discussed in Thread: TIDA-01393 , CSD87381P I am designing a PMIC for the Zynq UltraScale+ MPSoC XCZU11EG, and I am confused about calculating the inductor, RILIM, and output capacitor values for BUCK1, BUCK2, and BUCK6…
Other Parts Discussed in Thread: AM6421 Hello,
Also, they are planning to connect below mentioned devices with AM6421 and would like to understand if they can be used.
Sl No
Interface/Description
Part Number
Alternate…
Part Number: TMS320F28P659DK-Q1 Other Parts Discussed in Thread: SYSCONFIG
Hello Team,
I am unable to locate the exact CAN pins in SysConfig. The expected pin configurations should be either GPIO36 and GPIO37 or GPIO4 and GPIO5.
Could you please…
Part Number: MSP430FR2433 Hello,
I plan to use ADC to monitor Vref+ (1.2V).
ADC channel A4 can be selected to monitor this voltage internally.
This 1.2-V reference voltage could also be output to I/O pin P1.4 by setting the corresponding PMM control…
Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: UNIFLASH Hello Team,
One of our customers purchased 1 unit of P/N: IWR6843AOPEVM and reported an issue while using UniFlash with the part. They state the following,
------------
The software…
Hello,
For an application, I am looking for an adequate ADC and I would like to know which parameters I should consider and how I should interpret them to calculate the final error. I am measuring an NTC which full range voltage ranges from 65mV to…
Part Number: MMWAVE-STUDIO-XWRL68XX Other Parts Discussed in Thread: IWR6843AOP , UNIFLASH Hello,I would like to consult the following questions
My current environment adaptation is as follows
Hardware:IWR6843AOP
Software:mmwave_sdk_03_06_02_00…
Part Number: AWR6843ISK Other Parts Discussed in Thread: AWRL6844 , AWR6843 , AWR1843 Dear TI support team,
i m using AWR6843ISK team and able to Run TI-outofbox demo using AWR6843ISK+mmwavebooster on CCS debugger mode.
My requirement:
I want to…
Part Number: SN74ALVC164245 Other Parts Discussed in Thread: SN74LVC8T245 , Hi Team,
I have 5V CPCI signals which need to be level tranbslated to 3.3V CPCI signals.
My board have space contraints. So please suggest smaller possible size LVT.
Also…