Part Number: SK-TDA4VM Hi
I am simply just trying to check if the board has a Wi-Fi connection established to my network. I have been successful in the past trying to do so by using the "iw wlp1s0 link" command, however when I run the command now I…
Other Parts Discussed in Thread: CC2500 , CC2530 , CC2590 , CC1190 , CC2591 This presentation covers antenna theory, antenna measurements, range estimation and antenna support documentation.
Regards, Richard
Other Parts Discussed in Thread: MSP430FR5969 , MSP-EXP430FR5969 Hello chaps.
I am facing a strange bug/problem with an MSP430FR5969.
I am using the MSP-EXP430FR5969 Launchpad.
The code I am using is a modified "Out Of The Box Demo". At the beginning…
Jeff Tenney said: This morning I have discovered that one of the slave SPI devices has an _undocumented_ bus keeper on MISO @ 35K ohms That's very strange. No slave should have anything on MISO if it isn't chip selected. It shiould go high-impedance.…
Hi,
Attached the panel spec.
Another point is what's the dsi clock we should set from CPU side,
On imx95 device tree:
This's the 1366x768 clock setting, but we can not find a right setting for this 4K panel, CPU vendor suggest we need to check…
Part Number: UCC28C44 Tool/software: WEBENCH® Design Tools
I would like to check an application about the UCC28C44, as attached schematic, I would like to check several component whether could replace or not
Rstartup1 & startup2, 10.2 Kohm into…
Currently, we have made our own 20-pin ARM to 14-pin TI emulation adapter to verify proof-of-concept. Pins 9 and 11 of the 14-pin TI connector are shorted to tie the TCK and TCK return together.
I have a licensed copy of CCS V4.
I have setup the…
Part Number: LM76003 Tool/software: WEBENCH® Design Tools DEAR ALL,
The attached LM76003 DESIGN, output side 10.3uF capacitor is used. but in the market either 10uF or 12uF capacitor available. so can I use 12uF capacitor instead of 10.3uF? LM76003_based_design_Vin…
Other Parts Discussed in Thread: OMAP3530 Hi all,
I am trying to create a bootable SD card for my OMAP3530 EVM. For that I am following the following steps:
honey@honey-desktop:~$ sudo fdisk /dev/sdc
WARNING: DOS-compatible mode is deprecated…
Frantisek,
You can use the commands and procedure in the attached document to program the HEX data to the flash memory.
Tom
3173.Bq40z50 Data Memory Programming for Mass Production.pdf