Part Number: ADC08100 Other Parts Discussed in Thread: ADC081S051 Hi ADC team
Can I get information about ADC081S051CIMF CDM(Charged Device Model) on ESD?
We knew which HDM(Human Body Model) is 3500V on ADC081S051CIMF
Best Regards
Gerald
Other Parts Discussed in Thread: ADC08100 Hello,
I'm working on an application of the ADC08100 chip, and I noticed an error on page 15 of the datasheet. In the second paragraph, it states:
"The analog input signal that is within the voltage range set…
Ian,
The ADC08100 datasheet will have the voltage ranges for the data out pins. It will be in the electrical characteristics section of the datasheet.
Regards,
David Chaparro
Part Number: TLK2201B Other Parts Discussed in Thread: TLK1501 , , ADC08100 Hello,
I'm looking for a chip to convert the 8-bit parallel output from the ADC08100 flash ADC into a form that can be sent to a fiber optic transmitter (specifically the AFBR-59F3Z…
Part Number: LMH6628 Other Parts Discussed in Thread: TINA-TI , ADC08100 , THS5641A , Tool/software: TINA-TI or Spice Models Hi,
I'm making a isolated HV probe that is a ADC - ISO - DAC. I'm using ADC08100 - ISO7640 - THS5641A. Before the input to the…
Hi Grigorij,
Please find the EVM schematic and BOM attached here. These files will be uploaded to the ADC08200EVM in a few days.
ADC08060_ADC08100_ADC08200-SCH_A.pdf ADC08200EVM-BOM_A.xlsx
Best Regards,
Dan
Other Parts Discussed in Thread: ADC08060 , ADC08100 Could I run for example at 100MHz? 150MHz? Is there perhaps a graph of ENOB vs clock rate? Or does the ADC08060 fail catastrophically beyond 60MHz?
Hi Toby,
Initially, I would leave JP8 and JP9 in their default condition (1-2) since these set the fullscale input range of the ADC.
Are you applying an AC or DC signal at the analog input (VIN) in order to change the output codes? This EVM was designed…
Hi All,
I want to design a WiFi operated Smart LED Bulb with Standard AC input and Also need to control dimming via micro controller as well as will drive WiFi module also.
Can anyone suggest me any solution for these requirement.
Can you suggest me IC…