Part Number: ADC3221EVM
Signal generator outputs an up-ramp signal (100 kHz, 600 mVpp, like following graph), and feed to ADC3221EVM.
Said u p-ramp signal feed to CH1, ADC captured following waveform:
The same up-ramp signal feed to CH2, ADC captured…
Part Number: ADC3221EVM Other Parts Discussed in Thread: ADC3221 I am evaluating ADC3221 with ADC3221EVM and TSW1400.
Input clock to ADC3221 is from signal generator, sine wave, Vpp 1V.
When Input clock frequency > 22.53 MHz, the setup works. Although there…
Part Number: TSW1400EVM Default ADC3221EVM setting works with TSW1400, however, when I change ADC3221 to use 1-wire mode, this "frame clock error" pops up.
Is only default setting supported by TSW1400?
Part Number: ADC3221EVM Other Parts Discussed in Thread: ADC3221 , CDCE6214 , LMK03806 , LMK03318 TSW reports "Clock from ADC EVM is not received by TSW board":
USER_LED2 is on. Both EVMs are in default condition.
Part Number: ADC3221 Dear Specialists,
My customer is confirming ADC3221EVM and has a question.
I would be grateful if you could advise.
---
We're confirming ADC3221EVM
The register value of ADC3221EVM was read using ADC3000_GUI.
At that time, when…