Part Number: ADC32RF80EVM Other Parts Discussed in Thread: LMK04828 Hi team,
ADC32RF80EVM evaluation board uses a signal provided by the signal generator, which needs to be input into external clock input J5 and LMK04828 reference clock input J7 at…
Other Parts Discussed in Thread: ADC32RF80EVM , ADC32RF45 , ADC12DJ3200EVM , ADC12DJ3200 If there is a pulse signal whose frequency spectrum is 0-1GHz,can I use ADC32RF80EVM to sampling? how should i operate? In the HSDC pro ,when I use 4X decimation…
Other Parts Discussed in Thread: ADC32RF80EVM in the users' guide book,the voltage offerted for ADC32RF80EVM is 5v,what if out of the range? such as 5.16V, will does 5.16V do harm to the board?what is the maximum withstand of voltage ADC32RF80EVM ?
Other Parts Discussed in Thread: ADC32RF80EVM , LMX2582 , ADC32RF80 , LMK04828 Hello,
TIers!
I have a few questions about ADCRF80EVM. We use ADCRF80EVM to sample a square wave signal with duty cycle of 1% and repetition rate of 1MHz. The result is…
Other Parts Discussed in Thread: ADC32RF80EVM Hello,
For ADC32RF80EVM, what's the dynamic range of ADC32RF80EVM? What is the maximum and minimum voltage that can be input?I didn't find them in the data sheet.
Best regards,
David
Other Parts Discussed in Thread: ADC32RF80EVM , ADC32RF80 Hello,
We refer to the ADC32RF80EVM guide book, the fifth part is about EVM board examples.In this example, ADC channel-1 input frequency is set to 1.96GHz, NCO frequency is 1.9GHz, in software…
Other Parts Discussed in Thread: ADC32RF80 What does the Dual Band and Complex mean and when should I choose them?Can I use ChA and ChB at the same time to sample, what should I set in the GUI when I use the two channal in the same time?
Other Parts Discussed in Thread: LMK04828 , ADC32RF80EVM , ADC32RF80 , ADC12DJ3200 Hello!
When ADC32RF80EVM evaluation board uses external clock, it needs to divide a signal into two channels and input it to external clock input (J5) and LMK04828 reference…
Other Parts Discussed in Thread: LMK04828BEVM , ADC32RF80EVM , LMK04828 , LMX2592 , ADC32RF80 I connect the CLKin* of LMK04828BEVM to signal generator and set the frequency to 122.88MHz and connect the DCLKout0 and DCLKout10 to J7 and J5 of ADC32RF80EVM…
With regards to using ADC32RF80EVM with TSWJ5x boards: yes you can use J57 board instead of J56 since the max SerDes rate (out of ADC32RF80EVM) is 12.5Gbps or lower. J56 supports a SerDes rate up to 12.5Gbps whereas with J57, it can be as high as 15Gbps…