Part Number: ADC3424 About SDOUT pin, it output the read data in Serial Register Read operation.
But, according to datasheet, when it doesn't output data, it is set to High-impedance.
Then, we think it may cause the damage to connecting device (FPGA…
Part Number: ADC3424 Could you tell me the serial interface spec of ADC3424?
According to ADC3421-24.pdf P48 Table6,
fSCLK = 20MHz MAX
tDSU = 25ns min
tDH = 25ns min
But, when fSCLK = 20MHz, this clock time (tSCLK) = 50ns,
and if 50% duty, clock high…
Part Number: ADC3424 Other Parts Discussed in Thread: THS4551 , Hi team,
We designed custom board with ADC3424. We tested the interface with test patterns and they are okey. But when we tested the adc with short the input pin with VCM. All channel had different…
Part Number: ADC3424
The definition of the temperature range is defined as 140-85 ℃ in TA(air). What is the definition of TC (Case Temperature)? At present, thermal analysis simulations have shown that the case temperature (TC) of the ADC slightly…
Part Number: ADC3424 Other Parts Discussed in Thread: , TPS7A20 Hello,
I'm looking to use the ADC3424 and currently looking at the power supplies I provide for it. From Figure 121 of the datasheet I notice PSRR is generally 30-40dB across the frequency…
Part Number: ADC3424 Other Parts Discussed in Thread: ADC34J24 , Hi,
Do we have MCU/DSP MCU or DSP with LVDS or JESD204B port that is compatible for ADC3424/ADC34J24?
Customer is having hard time using the FPGA.
Thank you.
Regards, May
Part Number: ADC3424 Hi,
ADC3424 is designed in my product and found that some chips may have offset error which make the digital O/P too large and result a failure rate in production. My questions as below:
1. How to measure the offset error of ADC3424…
Part Number: ADC3424 Hello,
I am having identical issues to those outlined in the 'Test Pattern Confusion' thread that this post references.
I am running an ADC3424 at 40 MSPS, resetting it on power-up, enabling two wire mode, enabling test mode…
Part Number: ADC3424 Hi guys,
I'm designing a 4 channel amplifier with ADC circuit using the ADC3424 and in the datasheet it recommends an input circuit that it says should be designed to minimise insertion loss. Would it be sensible to change the values…
Part Number: ADC3424 Hi team,
We are penetrating our AMP+ADC solution to my customer. And we find that some noise is monitored in VIN+A and VIN-A pin when no signal is fed into ADC, see the red and blue curve. And the frequency is 100MHz, the same frequency…