Part Number: ADC3643EVM Hello, I would like you to confirm about below. * According to schematic of EVM, REFBUF voltage come from AVDD via J16(Jamper 16). However, it seems that input timing to AVDD pin and REFBUF pin is same. According to datasheet 10 Initialization…
Part Number: ADC3643EVM Hello, I'm looking for GUI tool for ADC3643EVM. Then, I found following E2E thread. (8) ADC3541EVM: Where can i download ADC35XXEVM GUI software? (Not HSDC Pro) - Data converters forum - Data converters - TI E2E support forum…
Part Number: ADC3643EVM Hi,
The datasheet of ADC364x gives a couple of examples for sampling giltch filter design for the input frequency range: DC to 30MHz, and 30MHz to 70 MHz.
In my case, the input frequency range is about 380MHz to 400 MHz.
What would…
Part Number: ADC3643EVM Hi,
According to the schematics of ADC3643EVM board (sbar014a.zip), ADC3644 is used.
I can't find the datasheet for such ADC. Is this ADC3644 the actual component mounted on the board?
If so, can you please provide the datasheet…
Part Number: ADC3643EVM Hello,
I am considering to user ADC3643EVM and connect it to a Xilinx FPGA evm board. For that, I would use the interposer board included with ADC3643EVM.
I want to check the connection between the ADC3643EVM and the FPGA EVM,…
Part Number: ADC3643EVM I have problem in components reference numbering in ADC3643EVM board. They are not matching schematics.
For example we wanted to connect FPGA_CLK for sampling clock. From schematics it can be understood that zero ohm resistor…
Part Number: ADC3642EVM Hi,
Yes you mentioned you would update the page to include a reference design? Can you please add a reference design for the ADC3642EVM.
Cheers
Part Number: ADC3642EVM Hi Team, Can we request for the design files of the ADC3642EVM for our customer? Unlike the ADC3643EVM, it seems that it isn't available in its product page. Thanks in advance! Kind Regards, Jejomar
Part Number: TSW1400EVM Hi Team,
Can you help troubleshoot the customer EVM issue below?
The customer tried the TSW1400EVM board to evaluate ADC3643EVM and DAC3162EVM boards. they believe that the problem is with the 1GB DDR module on the TSW1400EVM.…
Hi,
The image on the left is the most correct since the differential input pins (AINP and AINM) can swing from +1.125V to - 1.125V. The differential signal swing is (+1.125V - (-)1.125V = 2.25V). These voltages must both include the +0.95VDC common mode…