Part Number: ADC3660 Hi,
I have an application where I use 16 of the ADC3660 connected to an FPGA in 32 decimation/20bit complex mode. All of the ADCs have their NCOs at the same frequency and are configured identically. I would like to synchronize…
Part Number: ADC3660 We are using the ADC3660 in one of our new designs, and are having difficulty trying to calculate/specify the latency and propagation delays through the device.
We are driving DCLKIN and CLKP with synchronized, 40.96MHz clock signals…
Part Number: ADC3660 Hi,
Is the SYNC pin on the ADC3660 designed so it can be toggled every 64 clock cycles and not cause discontinuities or muting of the signal? I am not sure how I should interpret this line in the datasheet. I tried the sync via…
Part Number: ADC3660 Hello,
I'm checking ADC3660 datasheet.
This is its parameters.
- input full scale : 3.2Vpp
- input common mode voltage : 0.95V
- VREF : 1.6V
With a differential driver IC, I have designed following.
- Vocm for the driver…
Hi Delaney,
There have been a few customers that I know of, that have used the AM57xx Sitarra family for the ADC3660 (in serial CMOS mode using the McAsp interface). They have also utilized decimation to improve performance and reduce the ADC output…
Hi Delaney,
Yes, we have customers who are using the AM57xx in their systems, and we are working on a reference design for the ADC3660 and AM57xx. It looks like March of next year for a release of the reference design.
In terms of the DRA821, this…
Part Number: ADS5562 Other Parts Discussed in Thread: ADS5560 , ADC3660 Tool/software: Hello
We are considering using the ADS5562 for a new project development and i have questions regarding this component:
- It seems to be "active" in the availability…
Part Number: ADC3660EVM Other Parts Discussed in Thread: ADC3660 , CDCE6214 Tool/software: Hi team,
ADC3660 DCLKIN is from CDCE6214 OUT4_P, which is labeled InternalDCLKIN_P.
What is the output format and voltage on InternalDCLKIN_P? I'm concern because…
Part Number: THS4541 Other Parts Discussed in Thread: ADC3669 , , ADC3660 Hi,
I am using THS4541 for AFE to ADC3669
Kindly review my layout for any blunt flaws, i have followed EVK layout, yet wish to get some comments from experts