Part Number: ADS1015 Other Parts Discussed in Thread: ADS1014 Hi,
The customer uses ADS1015 to collect the single-terminal signal of the power supply voltage.
The input pin uses AIN0 and AIN1. How to configure the AIN2 and AIN3 pin of ADS1015, whether…
Part Number: ADS1015
Hi TI expert
Could you pls help to explain how to define the formula to measure the voltage input on ADC channel.
Add more information: we want to measure one voltage with upper limit is 3.3V connect with AIN0, then which FSR shall…
Part Number: ADS1015-Q1 Hi Expert,
May I know what is the role for C1/C2/C3/C3 here?
the capacitance with 4.7nF in AIN pin, Can we use 1nF or 10nF instead?
Thanks!
Ethan Wen
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi team,
Could you please advise the R and C below of ADC1015-Q1 internal Sample and Hold block?
I plan to add an external capacitor to compensate high impedance source and I would like…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 Hi team,
When the customer involved ADS1015-Q1, they found that the read failed in step 3 according to the Quick Start configuration. What is the possible cause?
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1115-Q1
Hi, Support Team
We have use ADS1015-Q1, but Resolution (Bits) and Number of input channels is not enough.
Could suggest other patrs for reference?
Support I2C/ 12bit ADC output voltage…
Part Number: ADS1015-Q1 Other Parts Discussed in Thread: ADS1015 HI TI expert
Here is query about the ADS1015 single-end config :
User sernario : AIN0~3 need work in the single-end mode ,but in config register MUX[2:0] seems can only config one pin mode…
Hello Daniel,
Apologies for the late response here, there was some movement in the team, and it seems this post was overlooked.
Unfortunately we do not have knowledge of Linux and subsystems. You will need to confirm that the subsystem is compatible with…
Part Number: ADS1015 Hi team,
Confirm two simple pieces of information: (1) Whether the detection voltage range of the chip is the following information?
(2) Is there flag bit for 12bit data?