Part Number: ADS1194 Tool/software: Hi there,
What is LEAD, Electrode and channel present in ECG AFE?
In ADS1194, the description shows it was 3 lead, 5 lead or 6 lead patient monitoring system . But there is only four channels present in AFE.
Is the Electrode…
Part Number: ADS1194 Other Parts Discussed in Thread: ADS1298 We reference the ADS1194/1198 datasheet. But our ADS1194/1198 has an overcurrent issue. Could you check my schematic? Thank you. I attach our schematic pdf in a comment.
We connected the device…
Dear Sir,
Thanks for your reply and support.
1. Which method do you use referring to datasheet page 57 - "two measurement procedures to determine the RLD electrode connection status using either a current or a voltage pull-down resistor, as shown in…
Part Number: ADS1194 Other Parts Discussed in Thread: ADS1196 , ADS1198
Hi Team,
Good day! We need your help. Customer is using ADS1194, on one device ADS ID is showing c, d,0,8, etc..it should show B4 according to per the datasheet.
Please find attached…
Part Number: BOOSTXL-CC2650MA Other Parts Discussed in Thread: ADS1194 , CC2650MODA , CC2650 , LAUNCHXL-CC2650 Tool/software: Code Composer Studio Hello,
I am a student working for a project using the BOOSTXL-CC2650MA.
I would like to program the CC2650MA…
Part Number: ADS1194 Hello, i bought an ECG 2 click board where the test signal looks ok, after that i made a custom PCB with the only diference that now AVDD = 3.3V, i tried the test signals in two of these custom boards and the signal have a big offset…
Part Number: ADS1198 Other Parts Discussed in Thread: ADS1194 Tool/software: I am using the ADS1198 with DMA. I configured the chip in RDATAC mode and am able to get data frames of 19 bytes.
Now I want to read multiple frames at once so that I can process…
Part Number: ADS1194 Hi,
When readout the 4 serial channels on ADS1194 and send it to a monitor, the signals are floating up or down if some movements happen. Is it possible to stabilize the readout more from the serial channels without losing signal…