Part Number: ADS1210 Hi,
Let me post as below about reset timing of ADS1210 the other day.
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/p/627987/2315621#2315621
After that, I also have studied other similar devices, ADS1212…
Part Number: ADS1210 Hi,
I would like to ask you a question about "reset timing" of ADS1210.
I have found that the reset timing that is defined at "old data sheet" is different from the latest one as below.
The old one needs "3 pulse…
Part Number: ADS1210 Hi,
Could you tell me how to calculate OCR and FCR of ADS1210?
If you have something equation to calculate OCR/FCR, please let me know.
Thanks and Best Regardds,
Part Number: ADS1210 Hi ,
My customers read the FCR register (upper 16 bits,Byte2 and 1) for each data rate.
・10Hz・・・ 6916h OK ・20Hz・・・ 68C3h OK ・40Hz・・・ F30Dh NG ・50Hz・・・ AF29h NG ・55Hz・・・ E74Dh NG ・60Hz・・・ AF29h NG
Is it correct to refer…
Part Number: ADS1210 Let me ask you a basic question.
In case of inputting out of range analog signal to "Ain" pins, what will happen?
1) in case of the input is out of spec, under absolute max range.
For example, Analog input signal is from…
Part Number: ADS1210 Hi,
Let me ask you a question about data shift phenomenon of ADS1210 as below.
The ADC output code is shift (red circle) as following graph when input is adding from 1mv to 1.4mV to ADS1210.
Have you ever experienced this kind of phenomenon…
Part Number: Hi,
Let me ask you following questions about Vref/Vbias, Xin specifications.
1) Vref
The Vref value of the specification is from 2.4V(min) to 2.6V(max), and the temperture specified is from -40 to +85℃.
My question is that the Vref value…
Part Number: ADS1210 Hi,
Let me ask you the procedure to issue "calibration" command.
Is it possible to issue the command to initialize ADS1210 setting and do calibration at the same time?
That is to say,
After setting(writing) INSR, continue to…
Part Number: ADS1210 Hi,
My customer is using ADS1210. He has a issue. It is A/D covert value is shift at being high temperature. The input differential voltage (AINP-AINN) is 0.193V. In case of 25 degrees, convert value is "4B4477h". In case of…
Part Number: ADS1211 We are using the ADS1210, and last spring it was active, but it became obsolete with a relative short last time buy period. The datasheet for ADS1210 also specifying the ADS1211. It seems like only footprint is necessary to change…