Part Number: ADS122C04 Hey guys,
Recently we've been trying out the ADS122c04 in some applications, and recently we've been trying to make some Pyranometer readouts.
Due to a request from the final client, there are no biasing resistors on the…
Part Number: ADS122C04 The ADS122C04 data sheet says to bypass the PGA in single ended mode. In our single ended photodiode application, enabling the PGA seems to reduce noise (possibly due to the internal chopper amp?). What are the consequences of using…
Hi Shinichi,
I measured the currents using a DMM in current measurement mode so the direct current measurement is going to be an average. I did not see any issues when powering the ADS122C04. I then set the register settings to the same values used by…
Part Number: ADS122C04 Hi,
We would like to use the continuous conversion mode of the ADS122C04 to implement interleaved sampling of three channels. It seems that we can implement this by first configuring all the configuration registers and then only…
Part Number: ADS122C04 Hello.
I am developing a product using the ADS122C04 device. I would like to use the "System Monitor" function to implement the self-diagnosis function. I have set up the internal multiplexer to measure analog power supplyy…
Part Number: ADS122C04 We are considering using the ADS122C04IPWR for the following system:
Three analog channels that have a bandwidth of < 40 Hz with common reference channel
Single ADS122C04IPWR for measuring the three differential analog channels…
Part Number: ADS122C04 Hi Team,
Good day.
I have a question about the ADC ADS122c04. How long does it take in turbo mode at an output data rate of 1200 to measure all 4 inputs once?
Or how long does it take to switch from one input to the other. So how…
Part Number: ADS122C04 Other Parts Discussed in Thread: ADS1015 Hi team,
My customer is using ADS122C04, do we have Linux driver for this part?
We found some drivers here, could you advise which one we can use for this part?
Thank you.
Part Number: ADS122C04 Hello everyone!
I am using ADS122C04 on a new project, and I have had problems with the PGA. I put 3.3V voltage both digital and analog, both using the same GND. I use an external 2.5V VREF. But I also tried using the internal VREF…