Part Number: ADS125H02 Other Parts Discussed in Thread: ADS124S08EVM , ADS124S08 I look for a single chip for 0-20mA,4-20ma,0-1V,0-5V,0-10V etc analog inputs and RTD and thermocouples.
I want to measure these sizes optionally on a single board. I found…
Part Number: ADS125H02
Hi
Please let us know the terminal connection for the 4~20mA and 0~10v dc for sensor measurements
Thank you in advance.
Regards
Thiagu
Part Number: ADS125H02 Team,
My customer accidentally connected 8V to the reference REFP0-input of the ADS125H02 via a 1k1Ω-resistor.
table 7.1 Absolute Maximum ratings in the datasheet mentions that the input and output pins of the device are diode -clamped…
Part Number: ADS125H02 Hi team,
For table 47, ADC Drift Error, is it calculated based on gain is 0.1875? While taking gain drift as calculation example, it is 4ppm/C*105C*(2*2.5/gain)*e-4/(2*2.5/gain)=0.042%, which is not 0.032% shown in table 47. Could…
Part Number: ADS125H02 The silk screen information of this material specification is ADS, but the actual material silk screen we received is XDS, please check whether this is the wrong material, or the silk screen has changed.
Hi Bella,
I spoke with our program management and quality teams, and it appears that these specific devices were improperly marked as prototype material ("XDS" instead of "ADS"). However, the devices you have shown in the first post are full production…
Part Number: ADS125H02 How does the Auto-Zero function affect the effective noise bandwidth?
Section 9.4.2 Auto-Zero Mode describes that the digital filter notches remain in the same locations, but the system has latency equal to the Conversion Latency Time…
Part Number: ADS125H02 Hi,
I am using this ADC to calculate the voltages that are in the range of 0.9V to 12V.I am able to perform the offset and gain calibartion on the ADS125H02.
Offset calibration procedure:
I have enabled the Internal short to VCOM…
Part Number: ADS125H02 Other Parts Discussed in Thread: ADS131E08 , ADS131M04 , ADS1220 Hello,
I try to use the ads125h02 for a project and have some difficulties. I am able to read all internal registers, but can not write on them.
For example - Mode1…