Part Number: ADS1260 We are building a multi-channel temperature instrument with one ADS1260 per galvanically isolated channel (AVDD = 5 V, external ratiometric reference on AIN0/AIN1 across R_REF = 4.02 kohm). The question below concerns a single device;…
Part Number: ADS1260-Q1 I'm designing a pressure sensor circuit using the ADS1260-Q1. I'd like to use the internal ADC to amplifying my bridge circuit. The bridge circuit has the following parameters:
2.5V nominal
0-25mV FSR
I'm supplying the…
Part Number: ADS1260 Other Parts Discussed in Thread: ADS1261 Hi, Expert,
We have a few questions for ADS1260 design:
Need your help to confirm if ADS1260 and ADS1261 are pin2pin, except Ch number, others are same.
PIN7, 8,9 used for mode control…
Part Number: ADS1260 Other Parts Discussed in Thread: ADS1261 , ADS127L21B , ADS127L11 , ADS127L21 We are planning to use ADS1260 in our new design and we have below two different input voltages.
Does ADS1260/61 supports above two voltage inputs?…
Part Number: ADS1260 Other Parts Discussed in Thread: ADS1240 , Dear Sir,
With reference to the attached image, I would be grateful for any guidance wrt whether the response shown from the ADS1260B device is expected behaviour?
Essentially with a…
Part Number: ADS1260 Tool/software: Hello - we're using the ads1260 ADC in a circuit which is measuring current in a test environment. We've been seeing some issues with accuracy, especially at start up impacting the lower end of the current we are attempting…
Part Number: ADS1260
1) what is offset error of "ADC126x"?
2) Can i use this ADC part to measure the DC current across the Shunt, our application is to measure min 10uA onwards DC current.
3) will there any Analog Front End required?
4) What is…
Part Number: ADS1261-Q1 Other Parts Discussed in Thread: ADS1235 , ADS1260 , ADS1260-Q1 , ADS1261 Tool/software: Dear Support,
I would like to ask for your help in choosing a voltage reference/LDO for the ADS1235/ADS1260 converter as Vref. Rating: Automotive…
Part Number: ADS1260 Tool/software: Hi,
I am using the ADS1260BIRHBT on my board.
I want to communicate with it with SPI.
I think I did all right : CPOL = 0, CPHA = 1, reset/ PIN is high.
When I try to write a register (0x46 for instance), the…
Part Number: ADS1260 Tool/software: Hi team,
A customer has a question about the meaning of tsu(DRST) and th(DRSP). Is this correct to understand that the next conversion will not occur if the stop command is within 100 [ 1/fclk ] from the point of…