Part Number: ADS131E04 Good afternoon everyone,
I am needing help regarding this IC, even though it is mainly for power measuremenet i want to read 4 load cells simultaneously.
The load cells are connected to 5V, they have a sensitivity of 2mv/V so at…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131A04 , ADS131M04 , Hi Team,
Can you help with the inquiry below?
I understand that this ADS131A04 device has no PGA integrated and t he gain that is featured is implemented "digitally" which means…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131E08 We are using a ADS131E04 in 24bit 16ksps mode. The values we get seem to be valid on all channels apart from the occasional extreme outlier, but we can deal with those. But if we look at…
Part Number: ADS131E08S Other Parts Discussed in Thread: TMS320F28377S , , ADS131M08 , ADS131M04 , ADS131E08 , ADS131E04 , ADS131A04 Tool/software: Hi, TI expert
There is an inquiry from a customer regarding ADC (24Bit) recommendation.
- Application : Fuel…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131E08S , ADS131A04 We have used ADS131E04 ADC in our one product. I would like to reuse same for another product we are starting design. Only one parameter is not suitable as Power up timing of…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131E08 Hello,
I have to use ADS131E04 in order to acquire data from a 3-axes accelerometer. The sensor outputs data in the 0-1.8 V range (nominally 0.1 to 1.7 V), in single-ended mode.
What is…
Part Number: ADS131E04 Hi,
I've looked through the datasheets for all three types, and am curious which ADC would work best for measuring AC Power (120-347VAC, voltage-divided down) at 60Hz. Having a PGA is not a big concern for me, as I will put all…
Part Number: ADS131E04 Hi,
If any dip in the DVDD(3.3V) is happened to the IC, malfunctioning happening the timing.
above waveform shown the dip pattern for the IC. It lasts for only 80mS. and one more observation is the system behaves incorrectly if…
Part Number: ADS131E04 Other Parts Discussed in Thread: ADS131M04
Hi,
I want to clarify some points regarding my input signal to ADS131E04.
ADS131E04 has a supply voltage of AVDD = 3.3 V and AVSS = 0 V. VREF is set to 2.4 V internal. Assuming gain is…