Part Number: ADS131M02 Hi I am using the controller reference code for ADS131M02 ADC. Using controller reference code, I have written code for processor I am observing the output is not updating with analog input for both channels.
Continuously getting…
Hi Kevin,
For the ADS131M04 (and below in channel count), the 1.2V reference integrated reference has no option for an external reference.
For the ADS131M06 (and higher channel count) there is an option to feed an external reference. That being said,…
Part Number: ADS131M02
Hello team,
My customer wants to synchronize the conversion timing of multiple ADS131M02.
Are below actions enough to accomplish synchronization of multiple devices? Is there anything else has to be done or missing settings to do…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M03 Hi Team,
Confirm one question: What is the input common-mode voltage when the ADC is a differential input? Thanks.
Part Number: ADS131M02-Q1 Hi Expert,
Thanks for your warm help!
Here are some question raised from me.
1. I use the excel of CS calculation sheet to calculate some parameter. Resolution(mA)=0.1/B3*1000. It seems that the resolution just has relationship…
Part Number: ADS131M02 Hello, we are wondering whether the ADS131M02 can be used in the following way:
interfaced via SPI pins (MISO, MOSI, SCLK, CS), but neither DRY or SYNC/RESET connected
modulator clock CLKIN generated by dedicated oscillator (not…
Part Number: ADS131M02 Hi
I have a project where I use a ADS131M02 AD converter together with an input ”amplifier” that actually is not an amplifier but a signal conditioning circuit.
The input is a tone signal in the range +10dBm to -60dBm…
Part Number: ADS131M02 Hi Team,
I want to ask a question that when I use ADS131M02 ADC with setting 24 bits length data, I want to read the register data if I need to send 24*6 clock to read it? Thanks.
Part Number: ADS131M02 Hi Team,
I am looking for a pure single ended alternative to ADS131M02:
2-channel (single-ended or differential input)
sampling rate min. 500SPS
SPI interface with data ready output
SPI speed (ca. 2 - 10MHz)
24-bit, 20-bit also …