Part Number: ADS131M02-Q1 Hi Expert,
Thanks for your warm help!
Here are some question raised from me.
1. I use the excel of CS calculation sheet to calculate some parameter. Resolution(mA)=0.1/B3*1000. It seems that the resolution just has relationship…
Part Number: ADS131M02 Hi
I have a project where I use a ADS131M02 AD converter together with an input ”amplifier” that actually is not an amplifier but a signal conditioning circuit.
The input is a tone signal in the range +10dBm to -60dBm…
Part Number: ADS131M02 Hello, we are wondering whether the ADS131M02 can be used in the following way:
interfaced via SPI pins (MISO, MOSI, SCLK, CS), but neither DRY or SYNC/RESET connected
modulator clock CLKIN generated by dedicated oscillator (not…
Part Number: ADS131M02 Hi Team,
I want to ask a question that when I use ADS131M02 ADC with setting 24 bits length data, I want to read the register data if I need to send 24*6 clock to read it? Thanks.
Part Number: ADS131M02 Hi Team,
I am looking for a pure single ended alternative to ADS131M02:
2-channel (single-ended or differential input)
sampling rate min. 500SPS
SPI interface with data ready output
SPI speed (ca. 2 - 10MHz)
24-bit, 20-bit also …
Part Number: ADS131M02
Hello team,
Is it possible to use SYNC/RESET pin to synchronize ADS131M02 and ADS131M0 4 (4ch version) at the same time?
Best Regards,
Kei Kuwahara
Part Number: ADS131A02 Other Parts Discussed in Thread: ADS131M02 Hi Team,
I have some concerns and need you to check when I design ADS131M02 ADC socket.
Can pin 11 SYNC/RESET not connecting to the MCU, just use RC reset at power on?
Can pin 13 DRDY not…
Part Number: ADS131M02
Hello Support team,
Customer ask if SPI command influence ADC sampling behavior, could you support? To receive data, if not NULL but RREG(1byte) or WREG(1byte) is used, are there any influence to sampling behavior or receiving…
Part Number: ADS131M02 Hello:
when I was using the ADS31M02 chip, I encountered an abnormal MISO phase of SPI communication, resulting in failure to decode data correctly
According to the manual, MISO outputs at the rising edge of the clock
The following…
Part Number: ADS131M02 Hello Support team,
Could you provide Production Distribution data of offset error and gain error? Customer request it.
Thanks,
Koji Ikeda