Part Number: ADS131M02 Hello:
when I was using the ADS31M02 chip, I encountered an abnormal MISO phase of SPI communication, resulting in failure to decode data correctly
According to the manual, MISO outputs at the rising edge of the clock
The following…
Part Number: ADS131M02 Hello Support team,
Could you provide Production Distribution data of offset error and gain error? Customer request it.
Thanks,
Koji Ikeda
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M04EVM , , ADS131M08EVM , ADS131M08 Hello Support team,
My customer is evaluating 50/60Hz voltage AC signal by using ADS131M04EVM, but, the peak to peak value on ADC result is smaller than measurement…
Part Number: ADS131M02 helllo:
There are two questions, hope you can help me,
Question 1 How is the response time calculated?
The default configuration: data output rate is 4K , external crystals is 8.19Mhz
When there is an excitation input, such as 1V…
Part Number: ADS131M02 Hello:
help me
Question: ADC data is stable for a long time,about 3ms. Is it normal?
Description:
ADC channel input: voltage change from 0 to 1.063V within 1ms,
ADC data output result: Read data through SPI communication…
Part Number: ADS131M02 Hello Support team,
Customer inquires internal clock on AMDS131M02. Does ADS131M02 have internal clock? Or does it always require external CLKIN for the conversion?
Datasheet 8.4.6 Current-Detect Mode show " The device uses an…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS127L11 Hello,
My customer needs the following specifications as mandatory ones and I think ADS131M02 is the best fit device, but it has 2 channels. Can it be used as a single-end input single channel…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS124S06 , ADS131M08 , ADS124S08 , ADS1248 , ADS1247 , ADS1261 , ADS1260 , ADS1220 , ADS122C04 TI has some ADCs (such as the ADS124S06 ) that are very well suited to ratiometrically measuring RTDs (4 wire…
Part Number: ADS131M02 We have the mikroe adc 15 board for testing and after setting everything up I started noticting only the irst readings were valid. After ~1.96seconds the board resets and we get 0xFF22 indicating a succesful reset. This seems to be…
Part Number: ADS131M02 Other Parts Discussed in Thread: ADS131M04 , Hi
If we done the fine tune on ADS131M02. can we use the same register settings on ADS131M04 to got the same performance?