Part Number: ADS131M06 Other Parts Discussed in Thread: ADS1220 Hi Team,
Our customer would like to clarify about the noise performance of ADS131M06. According to our customer,
I have a question regarding the noise performance of the ADC, part number ADS131M06…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS131A04 Hi Ryan,
Can you please help me with connections for Differentail inputs for ADS131M06?
I want to measure Line voltages (L1,L2,L3 with respect to Neutral).
I have checked application Information…
Part Number: ADS131M06 Hi team,
could you help to confirm whether our device could support REFIN to supply out side 1.2V application?
if yes, what is the drive ability? and any note for the application?
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS1262 , ADS1234
Hello
I have an application where I need 6 simultaneously analog inputs
2 loadcells
2 potentiometer
2 4-20mA sensors
for petentiometere I will connect the negative analog inputs to…
Part Number: ADS131M06 Hello,
The company I am working for is using the ADC ADS131M06 for sampling the output of a current transformer (CT) that has an integrated burden resistor, therefore outputting a voltage of 0.333V over relatively long twisted wires…
Part Number: ADS131M06 Hello,
I have problems with ADS131M06. On MCU boot, I am resetting it via SYNC/RESET, then sending WREG to clock register. Here I want these settings:
External clock source 8.192MHz
External reference voltage
All channels
250S…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS131M08EVM , AM2432
Hi Expert,
I am reading the datasheet of ADS131M06. I found the statement below regarding SPI clock and the modulator sampling clock.
8.3.5 Clocking and Power Modes The master…
Part Number: ADS131M06 Other Parts Discussed in Thread: ALLIGATOR Hello
See the figures bellow:
Figure 1: My circuit project - analog Front-End (Current).
Figure 2: Texas project - - analog Front-End (Current).
Figure 3: ADS131M06 6-Channel.
In Figure…
Part Number: ADS131M06 Hi, I've been running into an issue with the ADS131M06 where if I try to decrease Oversampling Rate to anything below 4096, I get data from the previous sample bleeding into the next sample for each channel. This has effectively…
Part Number: ADS131M06 Other Parts Discussed in Thread: ADS131M08 Hello Sir,
I wanted to measure following parameters for meterology project.
1) Voltages (L1-N, L2-N, L3-N, N-PE)-When neutral is present
2) Voltages (L1-PE, L2-PE, L3-PE)- When Neutral…