Other Parts Discussed in Thread: ADS4245 Dear Experts,
One of my customers is designing with our ADS4245 ADC using the LVDS interface and at 122.88MHz speed. They have some questions however about its interface due to some discrepancies in the datasheet…
I am using ADS4245EP Analog to Digital converter in my design with differential input signal and single ended clock. I am operating only one channel(channel B) in 2's complement parallel CMOS mode.At the initial power up of the ADC ,Clkout signal from…
Other Parts Discussed in Thread: ADS4245 Hi sir,
I use ADS4245 with LVDS output and SPI to control it.
I need ADS4245's output to be in tri-state at power up and i need to remove this state later with SPI.
Can i permanently connect CTRL1= high, CTRL2&CTRL3…
Other Parts Discussed in Thread: ADS4245 Hi! I have two questions regarding the ADS4245:
From table 7 in the datasheet, there is a chA standby chB active mode. What about chA active and chB standby, is this available?
I need to shut the ADC down when not…
Part Number: SM320C6748-HIREL Other Parts Discussed in Thread: ADS4245 Hi, We have DSP uPP_XD pins driven by ADS4245 port B and BOOT pins 2 and 3 are pulled up and the rest of the boot pins are pulled down to enable Flash Boot up configuration (BOOT[7:0…
Part Number: THS4521 Other Parts Discussed in Thread: ADS4245 , , THS4551 Hello,
In my project, I am using two ADC drivers THS4521IDR and an ADC ADS4245 and I would like to know how to connect them properly.
The input signal of the drivers comes from an…
Venu,
I would suggest looking at the ADS42xx family of data converter (12/14 bit, 65/125 MSPS). These are LVDS output devices. The maximum input swing is 2Vpp centered around a 0.95V common mode. Most of our converters will have a common max input swing…
Other Parts Discussed in Thread: TPS7A80 , DAC3484 , ADS4245 , ADS6145 What's the failure mode for TPS7A8001? If the failure mode is Vin short to Vout, then the input voltage will go to output, it can destroy load. How to protect it?
In my design 7 LDOs…