Part Number: TMS320C6748 Other Parts Discussed in Thread: ADS4245 Tool/software: Code Composer Studio I'd like to use EDMA3 on two 16-bit GPIO input data words. After reading about EDMA3, it seems straightforward, but I am not sure whether the volatile…
Part Number: LMH6554 Other Parts Discussed in Thread: ADS4245 Hello,
In my application the input IF is 30MHz, with 10MHz Bandwidth.
I am using LMH6554 in front of ADC. In data sheet figure 12, Harmonic Distortion for 30MHz, HD2= 102dBc and HD3 = 107d…
Part Number: LMH6518 Other Parts Discussed in Thread: THS4541 , , ADS4245 , VCA824 , LMH5401 , OPA859 , ADS4225 , THS3217 , OPA656 Hi,
I am building a differential probe and a scope with ADS 4225. I am willing to have the LMH6518 inside the probe so that it is…
Part Number: TMS320C6657 Other Parts Discussed in Thread: TMS320C6748 , , ADS4245
Hi, ALL
Now we will ready to measure DSP performance with high speed data converter.
DSP:
TMS320C6748
TMS320C6657
AD converter criteria:
1) resolution:12-14bit
2) sampling…
Other Parts Discussed in Thread: ADS4245 , THS4541 Hello,
I want to use THS4541 to drive an ADC ADS4245.
THS4541 is +5V supply.
I don't find the Vocm range in data sheet?
Does Vocm range depend to Supply voltage?
To match ADS4245 Vocm need to be 0.95V…
Other Parts Discussed in Thread: ADS4245 , ADS42JB49 , ADS42JB69 , ADS42LB49 , ADS42LB69 Hello!
I'm looking for a couple solutions that are pin for pin for the following:
14bit 65-80 MSPS ADC
16Bit 125 MSPS ADC
each solution needs 4 channels, and cost…
Other Parts Discussed in Thread: ADS4245 , SN74AVC16T245 , ADS4245EVM Hello,
I have an ADS4245 EVM. I want to use CMOS mode on this board which output from J1. In order to use CMOS mode, I just follow the datasheet 'User's Guide ADS42xx EVM' on page…