Part Number: ADS5407 Folks,
We've noticed that at power-up, the ADS5407's LVDS outputs are driven to approximately 1 Volt, even though the ADS5407's enable input is driven low. Is there any way that we can turn the LVDS outputs off or at least…
Part Number: ADS5407 Other Parts Discussed in Thread: LMH6553 Hello team,
I'd like to check if there is any concern or design notice for ADS5407 analog input when it is combined with LMH6553?
Thanks in advance. S.Sawamoto
Part Number: ADS5407 Folks,
We've designed the ADS5407 into a board at my company. We're using both ADC channels, and we're clocking the part with a fixed, continuously running 500 MHz clock. The A Channel of the ADC appears to work just fine…
Part Number: ADS5407 Other Parts Discussed in Thread: ADS54J66 , ADS54J54 , ADS54J64 , ADS54J64EVM , TSW14J57EVM Hello,
We need to update a module designed with ADS5407.
On this part, each channel has two interleaved ADCs operating at half the sampling rate…
Part Number: ADS5407 Other Parts Discussed in Thread: DS10BR254 , In my project, i have to synchronize 64 ads5407s on 16 platforms with K7(xilinx) fpga, and now i have such problems as follow: i have SYNC signal through a lvds buffer (DS10BR254) to link…
Part Number: ADS5407 Hi, Dear Supports:
I didn't find following information in the datasheet of ADS5407 (Dual Channel 12-Bit 500 Msps Analog to Digital Converter)., could help me?
1. In the default, what is the input voltage range?
2. In the default…
Other Parts Discussed in Thread: ADS5407 I am considering ADS5407 in an application where the clock frequency will be constantly changing up and down in the range 40 MHz to 500 MHz. From the data sheet it is not clear how this ADC behaves when presented…
Other Parts Discussed in Thread: ADS5407 This is in connection with thread ADS5407: How to read negative values from high speed ADCs - Data converters forum - Data converters - TI E2E support forums
Clock issues are raised seperately
1. Do i really require…