Other Parts Discussed in Thread: ADS5474 , ADS5402 , ADC12D500RF Hi,
I'm seeking for dual channels,12bits and over,400MSPS and over ADC with small latency like ADS5474. Would you provide the information ?
Best Regards,
Kato
Hi Amy,
Please see the update of our customer below.
The current for J12-J19 was about 316mA, the current for J14/J7 together was about 240 mA. The board was not modified. before I get no error from the HSDC, and the leds are lighting on TSW1400. but…
Other Parts Discussed in Thread: ADS5474ADS5474 on my board is clocked at 400MHz. When I analyzed the data from ADS5474 using FFT, I noticed that the noise floor is not flat. The noise floor is sloped down from DC to 200MHz. The noise floor at the DC…
Other Parts Discussed in Thread: ADS5474 , ADS5400 I notice that my ADS5474 output data has a DC offset about +5mV, which is about 37 codes above the zero output code. For a continuous sine wave input, the output data swings around output code 8229, not…
Other Parts Discussed in Thread: ADS5474 , ADS54RF63 , ADS5463 , ADS4129 , ADS4128 , ADS5402 , ADS54T04 Hello,
I am using ADS5474 for my system, but I am going to change a lower resolution (12bits) and low power consumption ADC.
Can somebody kindly give me a…
Other Parts Discussed in Thread: ADS5474 , LMK04816 Sir:
I need do a design with 4 ADS5474 to implement a interleaved ADCs, in which the sampling rate is 1.3G and each ADC works in 325M.
Now I have two clock schemes:
(1)One is used the dual PLL LMK04816…
Other Parts Discussed in Thread: ADS5463 , ADS5474 Hello forum!
I have a need for 14-bits of conversion at a widely and rapidly varying sample clock rate, from about 50MHz to 450MHz in under 10uS. The application might be OK with 12 bits, and in that case…
Hi,
We have not had to do this directly, but for a *few* ADCs synchronized I have seen it done. For example, there is the EVM with two interleaved ADS5474 at http://www.ti.com/tool/ads5474adx-evm and a similar EVM with four interleaved ADS54RF63 at http…
Other Parts Discussed in Thread: ADS5474 Hello,
I am testing ADS5474 for my ADC project for mobile communication.
Curently I am using 240MHz single input RF signal to ADS5474 pin 10 CLK and groung /CLK via a capacitor.
Input signal is about 0 ~ -2dBm…
Other Parts Discussed in Thread: AM3358 , ADS5474 , OMAP3530 Howdy,
I was looking at getting a Beagle Board xM with the TI AM3358 ARM processor and building a daughter board that has an ADS5474. The Beagle Board would probably be running an Ubuntu flavor…