Yes, I know, but I consulted the document "HSDCPro Automation DLL Manual" and the "TI_matlab_ADC" document, and found no applicable solution functions and methods, especially the working mode of ADC
Hi Jimmy,
Please see the Matlab Automation functions that are incorporated with HSDC Pro.
This thread may be helpful.
e2e.ti.com/.../2681919
Best Regards,
Dan
What i`ve already learned in chosing the right ADC-Driver is that it should have a Gain Bandwidth Safety Margin of 40dB, must be able to provide enough output current for the adcs input and must be able to deliver 3Vpp at the output to fit the fullscale…
Other Parts Discussed in Thread: ADS54J69 , ADS5482 Hello,
Kindly find below for my requirement for High Frequency ADC. Kindly share me ADC the part number for below requirement.
AC Performance
Sampling rate: Upto 500MSps (16Bit resolution)
…
Part Number: ADS5482EVM Other Parts Discussed in Thread: ADS5482 , ADS6445 Hi all Would you mind if we ask ADS5482EVM and ADS6445EVM? Our customer would like to use ADS5482 and ADS6445 using FPGA. If you have some software for these devices, could you…
Part Number: TSW1400EVM Other Parts Discussed in Thread: ADS5482 Dear team,
When use TSW1400 with ADS5482, data is stored in DDR of TSW1400, how can I directly read DDR data instead of saving it as a file and then reading it?
The function provided…
Also, do you think it is possible to connect the ADS5482 directly to an FPGA and do some signal processing there? This implies that the FPGA will be able to read the data coming out of the ADS5482, is that feasible?
Thanks,
Dinis
Part Number: ADS5482EVM Other Parts Discussed in Thread: TMS320C6657 , ADS5482 On hand I have both an ADS5482EVM and TMDXEVM6657L which I want to use for performance evaluation as core components in a new product design.
Direct interconnect of these…
Part Number: TMS320C6657 On hand I have both an ADS5482EVM and TMDXEVM6657L which I want to use for performance evaluation as core components in a new product design.
Direct interconnect of these two using the 6657's universal Parallel Port is not possible…
Hi Matteo,
Oh yes, good catch - you are correct. I used the NSD value for the ADC3561 (-150 dBFS/Hz). Yes please substitute the -158 dBFS/Hz for the ADC3563 into the equation.
I did a search with these parameters on our device page. I had to back…