Part Number: ADS58J63 Other Parts Discussed in Thread: LMK04828 I see that in Page 80h, register address 53h, bit 7 - it says enable "Divide by 2" for proper operation of ADS58J63.
Does it mean that I have to supply 1GHz clock to operate ADC…
Part Number: ADS58J63 Other Parts Discussed in Thread: ADS54J20 I downloaded the IBIS-AMI model for ADS58J63. I see two package model files in it namely - tx_package_DA0.s4p and tx_package_DA1.s4p.
I would like to know if these are the actual package…
Part Number: ADS58J63 Hi,
I am using ADS58J63 in my design. I was planning to do ground separation for Analog and Digital signal lines. I checked the EVM schematic and there no such separation is done. I see in the device pin diagram there are separate…
Part Number: ADS58J63EVM Other Parts Discussed in Thread: ADS58J63 Hi, I am using the ADS58J63 EVM along with the Xilinx ZCU102 EVM board. I am able to bring up the LMFS 4841 Mode0 configuration and it is working with ILAS. I want to replicate the same…
Part Number: ADS58J63
ZYNQ ZCU102 FPGA ADC(ADS58J63) EVM bring up is facing interfacing issues. The LMFS 4841 mode 0 configuration file provided by TI is not providing the required configuration. On loading the file in ADC GUI provided by TI, we are…
Part Number: ADS58J63 Other Parts Discussed in Thread: LMH5401 , ADC12J4000 Hi,
I am planning to use ADS58J63 in my design. I have a couple of queries regarding this.
1. The datasheet says the differential input full scale voltage as 1.9Vpp. Does it mean…
Part Number: ADS58J63 Hi,
I am designing a board having many ADS58J63 in a single board. Please let me know what is the requirements with respect to power supply like maximum ripple etc to achieve best possible performance out of the ADC.
Regards,
Ki…
Part Number: ADS58J63 I am using ADS58J63 in my receiver chain. My desired operating band is 250MHz to 500MHz. My application diagram is similar to what is provided in the datasheet (figure 140, pg 75). There is a differential gain amplifier before ADC…
Part Number: ADS58J63 Hi,
I am trying to configure my ADS58J63 for below configuration. Can you provide me a complete configuration file for this?
Configuration Details:
Mode: 0
LMFS: 4841
ADC Sampling rate: 491.2MSPS
Subclass: Subclass 1
Part Number: ADS58J63EVM Other Parts Discussed in Thread: ADS58J63 Dear team,
I have question about ADS58J63 when measuring with EVM.
When setting LMFS=2441, mode2, based on datasheet, we should write 0x01 to register 6A0016, but 204B could not be successfully…