Part Number: ADS7950 What is the REFP pin max current draw? Have an application with one source driving multiple ADC chips. Would be nice the info is in datasheet.
Part Number: ADS7950 In the datasheet of the ADS79xx I noticed that the sampling instance is defined in Figure 1 and Figure 51 in two different ways.
Figure 1 shows that the sampling occurs at the falling edge of not(CS), whereas Figure 51 shows that…
Part Number: ADS7950 Hi Team,
I want to use the ADS7950 in a battery powered device and wanted to clarify some information in the datasheet. The datasheet specifies a "Power-down state supply current" of 1uA. I want to clarify, is this the total power…
Part Number: ADS7950 we are planning to use an external 2.5V reference with 0.2% tolerance and will configure the device for 2Vref to sample 5V range input signals. however, i cannot find any details in the datasheet as to how accurate 2Vref is compared…
This would be at the falling of CS.
The datasheet, in the excerpt you pointed out is simplifying the process to explain the modes of the device. The timing diagram, figure 1, has a detailed timing diagram and section 8.1 details out the conversion cycle…
Part Number: ADS7950 Hi,
I want to know the way to read back the configuration settings from the ADS7950 to confirm that there is no change in settings during runtime. I could able to read only ADC data with channel information. Please help me on this…
Part Number: ADS7950 Could you please summarize or point me to a document that explains the differences between the two skews of the ADS7950S?
ADS7950SB
ADS7950S