Hello ,
I am referring to the code given in slaa397a for AES encryption - decryption .I am not
able to figure out that , with which standard mode of encryption/decryption (e.g. ECB )it is implemented.
Can anyone tell that , which encryption mode…
Part Number: CC2340R5 Other Parts Discussed in Thread: AES-128 Tool/software: Hello,
We are using the AES-CBC encryption on the CC2340R5. We would like to know the time it takes to perform AES-CBC encryption of 16-byte of plain text as per specification…
Part Number: MSP430F67791 Other Parts Discussed in Thread: AES-128 Tool/software: Hi TI,
Can we add the advanced DLMS functionalities into this EVM?
does 16-bit architecture is enough to include the above functionalities or it is for the basic DLMS…
Hi TI team,
I would like you confirm the following :
from CC26xx SimpleLink™ Wireless MCU Technical Reference Manual, 10.1.1 Functional Description:
******"The supported key length is 128-bit, which requires 10 rounds or 32 clock cycles"*******…
Part Number: SK-AM62 I am running some openssl speed tests on the SK-AM62 evaluation board . I am running PROCESSOR-SDK-LINUX-AM62X 6.1.46-g247b2535b2 . A chapter in TI’s processor-sdk-linux documentation discusses how to use the Cryptographic Hardware…
Part Number: LP-AM263P Tool/software: Hi Team , I referred 4 to 5 online calculators for aes 128 cbc encryption , none of them matches with the result provided in aes example code provided in mcu_plus_sdk . So , I need aes cbc 128bit encryption online…
Hello,
Using SDK8.6, not using SDK9.1 testing, currently found on SDK8.6:
1. Using the openssl speed command to test the algorithm performance, it is found that the speed of using software to process encrypted data is much faster than that of hardware…
Hi V.N.
We support EVITA light functionality for MSPM0G3507.
We support below hardware features for EVITA light:
1. TRNG (NIST SP800-22)
2. AES 128/256 for HW crypto algorithms (no key store, but could be stored in flash and protected)
B.R.…
Part Number: PROCESSOR-SDK-AM62X Hello,
We follow the link provided below to build and implement the hardware crypto accelerator supported on the AM62X platform. The hardware crypto accelerator driver exists and is loaded, but the hardware acceleration…