Part Number: AFE4490 Tool/software: Hi Team,
We're using AFE4490 in our application.
Shall we provide clock frequency of 8.192MHz instead of 8MHz to SPO2 AFE?
In datasheet, it was mentioned that the External clock frequency with 10% tolerance allowed…
Part Number: AFE4490 Tool/software:
What happens if you accidentally set the AFE4490 sample timing to be simultaneous when shifting it by setting it? The relevant section is Page 34 of the datasheet Figure 60. AFE Control Signals.
Part Number: AFE4490 Tool/software:
Hello TI Support Team,
We’re using the AFE4490 breakout PCB from Protocentral as our analog front-end for PPG, heart-rate, and SpO₂ measurements. Our host is an nRF52840 Development Kit. We started with the reference…
Part Number: AFE4490 Hello.
According to the datasheet, TX_REF value should be obtained as 0.75V, but the value obtained is 0V. The designed schematic is similar to the one provided in the development guide. The crystal oscillator output is obtained…
Part Number: AFE4490 Tool/software: I am experiencing the same phenomenon as in the bellow url. The settings on each board are identical. What is the possible cause? Is it that the voltage drop is within a range that cannot be detected by a tester?
…
Part Number: AFE4490 Tool/software: AFE4490 Output Voltage On a board with a AFE4490 mounted There were some that differed only in the program. As a result, there is a possibility that the output voltage (voltage between TXP and TXN) is different by about…
Part Number: AFE4490 Tool/software: Hi TIer
My customer use AFE4490 for SPO2 product many year.
Currently , we find a pcs of abnormal chip which have abnormal LED driver SPEC.
Could you give some suggestion? If the chip is damaged?
1. TX_REF is…
Part Number: AFE4490 Tool/software:
Greetings,
We are conducting research and development related to pulse oximetry and are using your AFE4490 pulse oximetry product.
We would like to inquire about the actual bias voltage applied to the photodetector…
Part Number: AFE4490 Tool/software: MPN:AFE4491NMAT Please help confirm will the security fuse be set to BLOWN before shipment? We've found that some are already in the BLOWN state during our current testing or are there other reasons that could cause…
Part Number: AFE4490 Tool/software: First Here is datasheet to use this case.
www.ti.com/.../afe4490.pdf
What I want to do: I want to set the AFE4490 datasheet Figure 116. LEDCNTRL: LED Control Register (Address = 22h, Reset Value = 0000h) and control…