Part Number: AFE4950 While monitoring the ADC value for the ECG signal, Can I perform lead detection through the AFE4950 Chip register setting?
If lead detection can be performed during monitoring, Can you tell me which of the 3 lead detection methods provided…
Part Number: AFE4950 Getting the eval board the AFE4950 (mother board) with the SFH7072 sensors - The sensor board supports 4LEDs, I am wondering can we replace this with a laser? Is there enough power for a 0.5W laser? If these are the electrical specifications…
Part Number: AFE4950 When register setting for AFE4950, Is it possible to set the register only at the beginning?
I want the registers to run while the program is running.
But it is impossible. Can't this chip set registers while the program is running…
Part Number: AFE4950 HI
When I tested, I found that the frequency response did not meet the requirements of IEC60601-2-47.
Is there a way to bypass the AFE4950 integrated high-pass filter?
Part Number: AFE4950EVM Other Parts Discussed in Thread: AFE4950
Hello
First of all, thank you for answering my last question.
Regarding the AFE4950EVM Kit, when is the AFE4950 Initialization Set Up applied? -> Is it initialized when power is supplied…
Hello Vadym,
We have a thread of correspondence via email. For further support, please ping us directly through there.
To reopen this thread, please reply to this post.
Kind regards, Nick Z
Part Number: AFE4950EVM Other Parts Discussed in Thread: AFE4950 Hello
First of all, thank you for answering my last question.
Regarding the AFE4950EVM Kit, when is the AFE4950 Initialization Set Up applied? -> Is it initialized when power is supplied…
Hello Guillaume,
Since we're in correspondence via email, I'll be closing this post since we're addressing the original question.
For further support please email me, or to reopen this thread reply to this post.
Kind regards, Nick Z
Part Number: AFE4950 Other Parts Discussed in Thread: AFE4490 Hi, I would like to use AF4490 for acquiring PPG signals with 6 LEDs.
Can someone confirm if I can get 1000 SPS with 6 LEDs?
Regards, Anurag