Part Number: AFE5832 Hi team,
My customer have one issue of AFE5832. All even channel and odd channel output has 180 phase delay.
See attached file for output waveform and register config. Other register is default. The input frequency is 3.5MHz and sample…
Part Number: AFE5832 Hi Team,
One of my customers have question below:
About the "Figure 19. DTGC Mode Test: Waveform" of following user guide www.ti.com/.../slou489.pdf
I thought the output signal should be same as the input. Why is the waveform…
Part Number: AFE5832 I have a custom AFE5832 board I am trying to test its SPI functionality. I am running the following test steps:
1. Software Reset : set address 0h to 0x0001 and SENe Low and SENo to High.
2. Write a custom ADC pattern: set address…
Part Number: AFE5832 Hi,
i have swaroop board with me and i have connected with phased array transducer. In GUI control im setting quick setup,i will click DUT HW Reset and click the Initialize device, then i will select the number transmitter and number…
Part Number: AFE5832 HI,
I have seen the application notes SBOA361.
I wonder if the board that is on demo is available for purchase? If not, is there any information or datasheet on that board design?
Thanks alot!
Yoon Hwee Leow
Part Number: AFE5832LP I have set the register C7H in device and have read out the data correct. but sample data have not change.
for example :
I set c7h 16'h0005
then set c7h 16'h0007
the wave I catch don't change
why the LNA GAIN and PGA…
Hi King,
Do you have access to EVM and GUI for AFE5818 and AFE5832? If you have installed these GUIs, then, the SPI config files for quick-start modes would be available in the below locations -
AFE5818 - C:\Program Files (x86)\Texas Instruments\HMC-DAQ…