Part Number: AFE7920 Hi, We are planning to use AFE7920EVM for our testing with Xilinx ZCU102 board.
Does this device have a Vivado demo file about JESD204B?
and,
When I try to use Latte to run bringup, it always reports 'FPGA RESET not detected…
Part Number: AFE7920 I am currently using the AFE7920 in combination with a ZynqMP SoC.
I have already successfully verified the signal loopback path in my system from RX to FPGA to TX . Additionally, I have confirmed that the TX port outputs the expected…
Part Number: AFE7920
Tool/software:
We are using the Latte release with API version 2.5. Our system is based on a custom board integrating the AFE7920 and Xilinx JESD204B IP, with the JESD interface configured in 8B/10B mode. While the JESD link can…
Part Number: AFE7920 Hi Team,
Posting on behalf of our customer.
I need support with chip documentation. I was wondering if there is a new version SBAU337_13th_May_2020 for AFE79XX chips. The one provided in the secure resources seems to be outdate…
Part Number: AFE7920 Tool/software: Hi~
We designed with af7920 and xilinx xcku3p, and confirmed SYNC in JESD TX/RX.
In the above situation, it was confirmed that the CW signal was generated in the FPGA and output from the RFIC, but when the CW of…
Part Number: AFE7920 Hello
We are using your newest C-library (CAFE 2p9) to calibrate the RX DSA. To be more precise, we are using its function "doRxDsaCalib(..)". As guide line we are following the procedure as descripted in the document "AFE79xx_RxDSACalibrationProcedure_Jun32019…
Part Number: AFE7920 Other Parts Discussed in Thread: AFE7903 We are using the AGC/ALC of the AFE79xx family. I saw this on a AFE7903. We got nearly everything running as expected. But the attack and decay timings are wrong set. If we measure the timing…
Part Number: AFE7920 Other Parts Discussed in Thread: AFE7903 We are using the AGC/ALC on a AFE7903 to switch the LNA. The behaviour was allways not as expected and we were unable to get it running also with your help. See https://e2e.ti.com/support/rf…
Part Number: AFE7920EVM Dear, I am testing the Serdes Eye feature using an AFE7920EVM board.
I am using both a Latte based script containing ' AFE.JESD.SERDES[0].getSerdesEye() , and a self written embedded application based on CAFE::tiAfe79_SerDes…
Part Number: AFE7920 Tool/software: Hello,
I have a question regarding the ADC input DSA control in the AFE.
The datasheet specifies a 25 dB range with 0.5 dB steps, but when I attempt to adjust the gain by 10 dB, the actual attenuation is only about…