Part Number: AFE7920 Tool/software: I am looking for a device spec/ datasheet with the min and max limits filled in for parameters like NF maximum allowable input power etc...
Many thanks
-Ray wallace
Part Number: AFE7920
i'm bringup afe7920 with xilinx zynqmp.
In latte, we got the settings we wanted and ZYNQMP wrote the settings to the AFE7920 via SPI. But the data coming from the AFE7920 to the FPGA is unchanged.
So I wanted to send something…
Part Number: AFE7920 Other Parts Discussed in Thread: AFE7952 Hello,
Are there any concerns or issues with developing on the AFE7920 & transitioning to an AFE7952 in the future?
Thank you!
Part Number: AFE7920 Hi,
What is the latest version of the AFE7920's API program? What I've been using is CAFE2p4. Also if there's a new one, please let me know how I can get it.
Thanks.
Part Number: AFE7920 hello i'm bring up my custom board with afe7920.
i need latte gui because config afe7920 many settings, how can i get latte gui.
i can't find this software
Part Number: AFE7920EVM Hi
The part number on query is actually not AFE7920EVM but AFE7920-0P7EVM. For some reason AFE7920-0P7EVM was not being "recognised" in the Part Number field.
SKU is AFE7920-0P7EVM was only recently added to our portfolio…
Part Number: AFE7920 Hi! I was wondering if there is any thermal data available for the AFE7920? I'm specifically looking for thermal resistance information (θJC and θJB) and the maximum junction temperature. Any help would be greatly appreciated…
Part Number: AFE7920 Hi.
I want to use AFE7920 in NR RF Repeater System.
but, latency of AFE7920 limits application of AFE7920.
Can I change interpolation filter coefficients for DUC and decimation filter coefficients for DDC of AFE7920.
If possible…
Part Number: AFE7920 Hello.
We are developing a Beamforming system using four AFE7920s.
After the initialization of the first AFE7920 is complete, we proceed with the initialization of the second AFE7920.
We perform the initialization of the four AFE7920s…