Part Number: AFE7920 Hi,
What is the latest version of the AFE7920's API program? What I've been using is CAFE2p4. Also if there's a new one, please let me know how I can get it.
Thanks.
Part Number: AFE7920 hello i'm bring up my custom board with afe7920.
i need latte gui because config afe7920 many settings, how can i get latte gui.
i can't find this software
Part Number: AFE7920EVM Hi
The part number on query is actually not AFE7920EVM but AFE7920-0P7EVM. For some reason AFE7920-0P7EVM was not being "recognised" in the Part Number field.
SKU is AFE7920-0P7EVM was only recently added to our portfolio…
Part Number: AFE7920 Hi! I was wondering if there is any thermal data available for the AFE7920? I'm specifically looking for thermal resistance information (θJC and θJB) and the maximum junction temperature. Any help would be greatly appreciated…
Part Number: AFE7920 Hi.
I want to use AFE7920 in NR RF Repeater System.
but, latency of AFE7920 limits application of AFE7920.
Can I change interpolation filter coefficients for DUC and decimation filter coefficients for DDC of AFE7920.
If possible…
Part Number: AFE7920 Hello.
We are developing a Beamforming system using four AFE7920s.
After the initialization of the first AFE7920 is complete, we proceed with the initialization of the second AFE7920.
We perform the initialization of the four AFE7920s…
Part Number: AFE7920 Dear Sir.
spur is measured at 760.32MHz on DAC port and ADC port.(Serdes line rate of DAC/ADC is 12.16512G and JESD204C is used)
12.16512G is a multiple of 760.32M.
I think that the spur can be related to Seredes line rate.
what…
Part Number: AFE7903 Other Parts Discussed in Thread: AFE7920 , Hello,
My customer wants to know if there is pin compatibility between AFE7903 and AFE7920.
If AFE7920 is replaced with AFE7903 on a board designed to use AFE7920, are there any anticipated…
Part Number: AFE7920 Hello.
First, I know how to run run-time DC-offset cal or to stop DC-offset cal.
# how to run time dc-offset calibration
SPIWrite 00a3,00,0,7
SPIWrite 00a2,01,0,7
SPIWrite 00a1,03,0,7
SPIWrite 00a0,0f,0,7
SPIWrite 0193,4b,0,7
…