Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7920 , AFE7950 Hi Team,
Would it be possible to provide S parameters for the EVM with AFE7920 on it, for revision A and B?
We currently have in our possession what we figured out to be revision…
Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7920 , Hi Team,
I was wondering if there is a way in Latte to log the content of LMK registers, in a manner similar to what is already being done with AFE7920 registers.
At the moment in my script…
Part Number: AFE7906 Other Parts Discussed in Thread: AFE7920 , AFE7950 , AFE7900 , We have lot of reference sch as reference with AFE7900, AFE7920,and AFE7950 to design AFE7906 and updated design is AFE7920 is developed in 2022 jul.
We want to make phase…
Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7920 Hi Team,
I noticed recently that on the TI secure folder are a couple of excel documents about AFE79xx matching networks, suggesting what kind of changes one should do to improve operation…
Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7920 , Hi,
I was wondering if it is possible to set up the AFE7920 eval board module in a repeater configuration, without FPGA board?
Kind regards,
Željko
Part Number: AFE7920EVM Other Parts Discussed in Thread: AFE7920 Hi Team,
I recently did an experiment with AFE7920EVM, where at the input of it's ADC A I bring 0 dBm signal @ 600 MHz, and then I measure the signal at the DAC A output.
DAC A NCO frequency…
Hi Zeljko,
This error usually occurs when the setup.py script is set for the AFE7900 device, as the VCO range is slightly different compared to the AFE7950 and AFE7920. One thing that you can check is that in the setup.py script you have set the chipVersion…
Zeljko,
Unfortunately both the AFE7920 and AFE7950 can only tolerate a signal up to 300mV over VDDIO before the device will be damaged. I checked the EVM schematics and we do not have any way to level shift the signal on the EVM, so you'll need to look…
Hi Farid,
The AFE7920 only supports complex DDC/DUC modes. The DDC/DUCs cannot be bypassed. So though the ADCs are sampling at 3GSPS and the DACs at 12GSPS, the BW of these channels is limited by decimation/ interpolation factor being used.
Regards,
V…
Other Parts Discussed in Thread: AFE7920 Hi Team,
SN1905509IABJ FIT and MTBF is not available online, can you please kindly provide the details.
Your prompt support would be highly appreciated, thank you!