Part Number: AMC1210 Other Parts Discussed in Thread: TIDA-01527 , ADS1205 , ADS8364 Hi team,
I find about two solutions about resolver decoding:
1.Using the AMC1210 in Resolver Motor Control Systems;
2.TIDA-01527
Now I look for a solution about 6 resolvers…
Part Number: AMC1210 Hello, I'm always stuck with my problem.
To answer Tom, the 'delay' is in the infinite loop so it doesn't depend on the interrupt.
The pin ACK acts the same with ou without the 'delay'.
Part Number: AMC1210 Dear Dataconverter experts,
how can the measurement time of AMC1210 be calculated. It seems not to be the settling time from the DS.
Example:
Sinc Order SST=3
SOSR=32
IOSR=8
f_mod = 16,67 MHz
(mit IMOD=0)
this would give a measurment…
Part Number: AMC1210 Hi E2E Good day.
How to properly terminate the following pins if unused?
AVDD -pin 10 IN4 - pin 8 PWMx -pins 11/12 ADx - pins21-28
Thank you for the help. Regards, Carlo
Hello Tom,
Thanks for your answer.
For the delay : the code that measures the current is executed in the infinite loop in the main function. When it has a measured value ready, the AMC1210 generates an interrupt on his ACK pin connected to the STM32.…
Part Number: AMC1210 Other Parts Discussed in Thread: AMC1303M2510 , , AMC1303EVM , ADS1202
Dear TI Team
Our customers are considering using the AMC1210.
I have been asked by them if there is an EVM that can be evaluated with the following circuit configuration…
Part Number: AMC1210 Hi,
my customer wants to measure the current on three phases with four of the integrated filters on AMC1210. The measurement must be done at exact the same time, to have it in relation to other meaured values of the system.
The…
Part Number: AMC1210 Other Parts Discussed in Thread: ADS1205 Hello I use the AMC1210 chip paired with the ADS1205 to measure the rotation angle of the transformer(RESOLVER). I have the following questions: 1) Can I get the initialization order of the…