Part Number: AMC1304L05 We're working on grid tie inverter & using AMC1304L05 for grid voltage & current measurement. We're seeing frequent failures of the device on grid voltage side. We're maintaining < 50mV at the AinP & AinN inputs @ 300Vac. Fig1…
Part Number: AMC1304L05 Other Parts Discussed in Thread: AMC1304L25 Do we have more specification data for LDO output Voltage at VCAP pin ?
- Iout max
- Ripple
- Tolerance
Part Number: AMC1304L05 Hello,
Please see the Functional Block Diagram in section 8.2. According to this diagram, part has diff opamp and Delta-Sigma modulator from the signal chain analyzing point of view.
I need define the accuracy the current measurement…
Part Number: AMC1304L05 Other Parts Discussed in Thread: DRV8301 , TIDA-00080 In my case, i'll use the amc1304 and drv8301 to drive the BLDC.
And I’ve read the sch of TIDA-00080 - ISE3010.
1. My question is why GND_USH1 and GND_USH are not same…
Other Parts Discussed in Thread: AMC1304L05 4. Add a new one.
In the amc1304 datasheet 7.1 Absolute Maximum Ratings
The Analog input voltage at AINP, AINN voltage is ( AGND – 6 to 3.7 ) V.
And in the 8.3.1 Analog Input
" There are two restrictions…
Part Number: AMC1304L05 Other Parts Discussed in Thread: TIDA-01349 Hi Team,
one of my customers is trying to develop a motor drive application that conforms to the IEC 61800-5-1 standard and the customer is planning to use the AMC1304L05 in the application…
Part Number: AMC1304L05 Hi Team,
One of my customers has a question about the AMC1304L05:
How does the part behave outside the linear range between ± 50mV and ± 62.5mV? Is there a graph or information on how the part behaves during a measurement in this…
Part Number: AMC1304L05 Other Parts Discussed in Thread: TIDA-01606 I am designing a three phase grid connected inverter by studying the TIDA-01606 reference design.
In yor design, you use a hall effect current transducer to sense the inverter side inductor…
Part Number: AMC1304L05 Other Parts Discussed in Thread: ISO224 , AMC1336 Tool/software: WEBENCH® Design Tools Hi team,
we have a requirement for ADC IC with below specification:
16-bit Resolution
Opto Isolated
1.5KV isolation, Power supply isolation,…
Part Number: AMC1304L05 Hi!
I m working with my inverter design. During the designe, i found a problem.
It is important to match impedance of LVDS interface for AMC1304 sensor? What value should it be? Where can I find such informations?
The lenght and…