Part Number: AMC1306M25 Hi Team,
The customer uses the AMC1306M25 to capture the phase current of the motor and the SIN3 filter generated by the FPGA to capture the data.
If the SINC3 filter is in continuous operation, the data sampling is as expected…
Part Number: AMC1306M25 Hi expert,
Customer is seeing our AMC1306M25. Due to AMC1306's AVDD power is not that stable in real products, for the figure 53, under what voltage for AVDD will trigger fail-safe mode? And what's the time delay for missing AVDD…
Part Number: AMC1306M25 Hi team,
I would like to know if the high and low CLKIN voltage are reasonable, as long as they meet the range in the following figure?
Thanks!
Regards,
Ivy
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1350 , Hi team,
Customer wants to know whether the offset error can have aging degradation. They need to know the offset error(+/-100uV min/max) can be increased in two or three times by aging…
Part Number: AMC1306M25 The application scenario is current sampling driven by motor servo,This is the diagram:
Encountered two problems:
There are burrs in the current sampled by the software when the motor is idling。
The sampling current of software…
Part Number: AMC1306M25 I want to use the Simulink model of AMC1306 for system-level simulation, but I can only download the IBIS model from the device webpage. How can I obtain or request the Simulink model for this device?
Part Number: AMC1306M25 Hi,
What is the UL number of AMC1306M25DWVR? Is it number for UL-US-L181974-14-02604102-3 on the attached file?
Please help to confirm, thanks~
sbaq007-amc1306.pdf
Hi Alexander,
Thanks for your reply. Customer tried implementing all the recommended suggestions but the saturation issue still persists. Please find their comments below.
1. When we individually test the IC with +/- 250mV at the inputs, we are getting the…
Part Number: AMC1306M25 Other Parts Discussed in Thread: AMC1305M25 , Hi,
in the datasheet of AMC1305M25 section 7.10 is shown Vclipping with 312.5mV Typ.
For AMC1306M25 it is shown with 320mV.
Are both values correct, if yes what's the reason for the…
Part Number: AMC1306M25 Hi Team,
Could you pls recommend suitable device of two-channel buffer for CLKIN and DOUT pin in AMC1306M25 device? Thanks.
Best,
Stanley