Part Number: AMC60304 Hello, Q1: Does AMC60304 itself automatically detect which interface, SPI or I2C, the connected master has? There is nothing users have to care about other than just connecting either SPI or I2C? Q2: When RESET_, CLR_/LDAC_ and…
Part Number: AMC60304 Dears
I have a project for Optical module 400G QSFP-DD DR4
need One laser support 4-way output so i need Idac>400mA.
Can AMC60304 IDAC two channels are combined into one channel, and the output reaches 400mA??
Part Number: AMC60304 Hi Sir,
Have features like AMC60304 but need 8-ch IDAC AMC series? for 100G optical transceiver module solution.
in addition, IDAC solution with following specification also require:
for 25G optical transceiver module,
1. 1-ch IDAC+4…
Part Number: AMC60804 Other Parts Discussed in Thread: AMC60304 Hi Sir,
may we know the pin define of AMC60804 and AMC60304 is the same? because seem is same package and body size.
can AMC60804 directly replace AMC60304?